我通过添加dcsm.cmd和dcsm.asm文件来进行加密,烧录成功后,重新给板子上电,用XDS200仿真器连接,每次连接都是弹出下图的故障,请问有哪些可能或原因,谢谢
.sect "dcsm_otp_z1_linkpointer" .retain .long 0x00003FFF .long 0x00003FFF .long 0x00003FFF .sect "dcsm_otp_z1_jlm_enable" .retain .long 0xFFFF0000 ;Z1OTP_JLM_ENABLE .sect "dcsm_otp_z1_jtag_pswdh" .retain .long 0x01234567 ;Z1OTP_JTAGPSWDH0 .long 0x03678901 ;Z1OTP_JTAGPSWDH1 ;; ;; .sect "dcsm_otp_z1_cmac_key" ;; .retain ;; .long 0x00000000 ;Z1OTP_CMACKEY0 ;; .long 0x00000000 ;Z1OTP_CMACKEY1 ;; .long 0x00000000 ;Z1OTP_CMACKEY2 ;; .long 0x00000000 ;Z1OTP_CMACKEY3 ;; .sect "dcsm_otp_z1_pswdlock" .retain .long 0xFB7FFFF0 .sect "dcsm_otp_z1_crclock" .retain .long 0x7FFFFFFF ;; .sect "dcsm_otp_z1_gpreg" ;; .retain ;; .long 0x5AFFFFFF ;Z1OTP_GPREG1 = Z1_BOOTPIN ;; .long 0x5AFFFFff ;Z1OTP_GPREG2 ;; .long 0xFFFFFF00 ;Z1OTP_GPREG3 = Z1OTP_BOOTDEF_LOW ;; .long 0xFFFFFFFF ;Z1OTP_GPREG4 = Z1OTP_BOOTDEF_HIGH .sect "dcsm_zsel_z1" .retain .long 0x20FFFFFF ;Z1OTP_CSMPSWD0 (LSW of 128-bit password) .long 0x0123FFFF ;Z1OTP_CSMPSWD1 .long 0x0FFFFFFF ;Z1OTP_CSMPSWD2 .long 0xFEEEEEEE ;Z1OTP_CSMPSWD3 (MSW of 128-bit password) .long 0x55555555 ;Z1OTP_GRABSECT1 .long 0x55555555 ;Z1OTP_GRABSECT2 .long 0x55555500 ;Z1OTP_GRABSECT3 .long 0x00005555 ;Z1OTP_GRABRAM1 .long 0xFFFFFFFF ;Reserved .long 0xFFFFFFFF ;Reserved .long 0xFFFFFFFF ;Z1OTP_EXEONLYSECT1 .long 0x0000FFF0 ;Z1OTP_EXEONLYSECT2 .long 0x000000FF ;Z1OTP_EXEONLYRAM1 .long 0xFFFFFFFF ;Reserved .long 0x60806688 ;Z1OTP_JTAGPSWDL0 .long 0x0125A2B5 ;Z1OTP_JTAGPSWDL1 ;---------------------------------------------------------------------- ; For code security operation,after development has completed, prior to ; production, all other zone select block locations should be programmed ; to 0x0000 for maximum security. ; If the first zone select block at offset 0x10 is used, the section ; "dcsm_rsvd_z1" can be used to program these locations to 0x0000. ; This code is commented out for development. ; .sect "dcsm_rsvd_z1" ; .loop (1e0h) ; .int 0x0000 ; .endloop ;---------------------------------------------------------------------- ; Zone 2 ;---------------------------------------------------------------------- .sect "dcsm_otp_z2_linkpointer" .retain .long 0x00003FFF .long 0x00003FFF .long 0x00003FFF .sect "dcsm_rsvd_z2" .retain .long 0xFFFFFFFF ;Reserved .sect "dcsm_otp_z2_pswdlock" .retain .long 0x1F7FFFFF .sect "dcsm_otp_z2_crclock" .retain .long 0x3FFFFFFF ;; .sect "dcsm_otp_z2_gpreg" ;; .retain ;; .long 0x5AFF1820 ;Z2OTP_GPREG1 = Z2_BOOTPIN ;; .long 0x5AFFFFff ;Z2OTP_GPREG2 ;; .long 0x00000000 ;Z2OTP_GPREG3 = Z2OTP_BOOTDEF_LOW ;; .long 0xFFFFFFFF ;Z2OTP_GPREG4 = Z2OTP_BOOTDEF_HIGH .sect "dcsm_rsvd1_z2" .retain .long 0xFFFFFFFF ;Reserved .long 0xFFFFFFFF ;Reserved .sect "dcsm_zsel_z2" .retain .long 0xFFFFFFFF ;Z2OTP_CSMPSWD0 (LSW of 128-bit password) .long 0x1F7FFFFF ;Z2OTP_CSMPSWD1 .long 0xFFFFFFFF ;Z2OTP_CSMPSWD2 .long 0xFFFFFFFF ;Z2OTP_CSMPSWD3 (MSW of 128-bit password) .long 0xAAAAAAAA ;Z2OTP_GRABSECT1 .long 0xAAAAAAAA ;Z2OTP_GRABSECT2 .long 0xAAAAAA00 ;Z2OTP_GRABSECT3 .long 0x0000AAAA ;Z2OTP_GRABRAM1 .long 0xFFFFFFFF ;Reserved .long 0xFFFFFFFF ;Reserved .long 0xFFFFFFFF ;Z2OTP_EXEONLYSECT1 .long 0x0000FFF0 ;Z2OTP_EXEONLYSECT2 .long 0x000000FF ;Z2OTP_EXEONLYRAM1 .long 0xFFFFFFFF ;Reserved .long 0xFFFFFFFF ;Reserved .long 0xFFFFFFFF ;Reserved
MEMORY { PAGE 0 : /* Program Memory */ /* Z1 OTP. Z1 password locations / Flash and RAM partitioning */ DCSM_OTP_Z1_LINKPOINTER : origin = 0x78000, length = 0x00006 DCSM_OTP_Z1_JLM_ENABLE : origin = 0x78006, length = 0x00002 DCSM_OTP_Z1_GPREG : origin = 0x78008, length = 0x00008 DCSM_OTP_Z1_PSWDLOCK : origin = 0x78010, length = 0x00002 DCSM_OTP_Z1_CRCLOCK : origin = 0x78012, length = 0x00002 DCSM_OTP_Z1_JTAG_PSWDH : origin = 0x78014, length = 0x00004 DCSM_OTP_Z1_CMAC_KEY : origin = 0x78018, length = 0x00008 /* DCSM Z1 Zone Select Contents (!!Movable!!) */ DCSM_ZSEL_Z1_P0 : origin = 0x78020, length = 0x000020 /* Z2 OTP. Z2 password locations / Flash and RAM partitioning */ DCSM_OTP_Z2_LINKPOINTER : origin = 0x78200, length = 0x00006 DCSM_OTP_Z2_RSVD : origin = 0x78206, length = 0x00002 DCSM_OTP_Z2_GPREG : origin = 0x78208, length = 0x00008 DCSM_OTP_Z2_PSWDLOCK : origin = 0x78210, length = 0x00002 DCSM_OTP_Z2_CRCLOCK : origin = 0x78212, length = 0x00002 DCSM_OTP_Z2_RSVD1 : origin = 0x78214, length = 0x0000C /* DCSM Z2 Zone Select Contents (!!Movable!!) */ DCSM_ZSEL_Z2_P0 : origin = 0x78220, length = 0x000020 } SECTIONS { dcsm_otp_z1_linkpointer : > DCSM_OTP_Z1_LINKPOINTER PAGE = 0 dcsm_otp_z1_gpreg : > DCSM_OTP_Z1_GPREG PAGE = 0, type = DSECT dcsm_otp_z1_pswdlock : > DCSM_OTP_Z1_PSWDLOCK PAGE = 0 dcsm_otp_z1_crclock : > DCSM_OTP_Z1_CRCLOCK PAGE = 0 dcsm_otp_z1_jlm_enable : > DCSM_OTP_Z1_JLM_ENABLE, PAGE = 0 dcsm_otp_z1_jtag_pswdh : > DCSM_OTP_Z1_JTAG_PSWDH, PAGE = 0 dcsm_otp_z1_cmac_key : > DCSM_OTP_Z1_CMAC_KEY, PAGE = 0, type = DSECT dcsm_zsel_z1 : > DCSM_ZSEL_Z1_P0 PAGE = 0 dcsm_otp_z2_linkpointer : > DCSM_OTP_Z2_LINKPOINTER PAGE = 0, type = DSECT dcsm_otp_z2_gpreg : > DCSM_OTP_Z2_GPREG PAGE = 0, type = DSECT dcsm_otp_z2_pswdlock : > DCSM_OTP_Z2_PSWDLOCK PAGE = 0, type = DSECT dcsm_otp_z2_crclock : > DCSM_OTP_Z2_CRCLOCK PAGE = 0, type = DSECT dcsm_rsvd_z2 : > DCSM_OTP_Z2_RSVD, PAGE = 0, type = DSECT dcsm_rsvd1_z2 : > DCSM_OTP_Z2_RSVD1, PAGE = 0, type = DSECT dcsm_zsel_z2 : > DCSM_ZSEL_Z2_P0 PAGE = 0, type = DSECT }
您好,
如果工作设置和非工作设置(CCS 版本、使用的.out文件等)之间没有差异,您能否确认在引导模式选择引脚上配置了等待引导?
在这种情况下,等待引导将允许您连接,但由于 ECSL 保护,闪存引导不允许。
您好,
你好,我用280039也遇到同样的问题,配置了Jtag的密码后,在wait模式下始终无法连接到CPU。通过在ccxml文件里用test connection测试jtag回路的连接情况是正常的。我的硬件状态是280039的dome板,仿真器就是dome板上的XDS110。
您的问题和贴主的问题还不是完全一样。
如果无法解决您的问题,请重新发帖专题讨论,感谢理解。