Part Number: TMS320F2800157
我们使用此universal_motorcontrol_lab_f280015x工程做电机硬件过流响应时间性能测试,发现U相、V相硬件过流响应时间为3.2us,W相硬件过流响应时间为28us,使用2800157芯片,此工程硬件过流配置为,使用芯片内部CMPSS比较器,通过epwmxbar将比较器信号引入epwm模块,通过DC和TZ子模块使PWM输出强制停止,如何配置可以缩短硬件过流响应时间,即从过流电流发生到pwm强制关断的时间缩短为6us以内?


CMPSS比较器配置如下:
// CMPSS - Three phase current
#define MTR1_CMPSS_U_BASE CMPSSLITE3_BASE
#define MTR1_CMPSS_V_BASE CMPSSLITE3_BASE
#define MTR1_CMPSS_W_BASE CMPSS1_BASE
obj->cmpssHandle[0] = MTR1_CMPSS_U_BASE; //!< the CMPSS handle
obj->cmpssHandle[1] = MTR1_CMPSS_V_BASE; //!< the CMPSS handle
obj->cmpssHandle[2] = MTR1_CMPSS_W_BASE; //!< the CMPSS handle
void HAL_setupCMPSSs(HAL_MTR_Handle handle)
{
HAL_MTR_Obj *obj = (HAL_MTR_Obj *)handle;
#if defined(MOTOR1_ISBLDC) || defined(MOTOR1_DCLINKSS)
#else // !(MOTOR1_ISBLDC || MOTOR1_DCLINKSS)
// Refer to Technical Reference Manual to configure the ePWM X-Bar
uint16_t cmpsaDACH = MTR1_CMPSS_DACH_VALUE;
uint16_t cmpsaDACL = MTR1_CMPSS_DACL_VALUE;
#if defined(HVMTRPFC_REV1P1)
ASysCtl_selectCMPHPMux(MTR1_IU_CMPHP_SEL, MTR1_IU_CMPHP_MUX);
ASysCtl_selectCMPLPMux(MTR1_IU_CMPLP_SEL, MTR1_IU_CMPLP_MUX);
ASysCtl_selectCMPHPMux(MTR1_IV_CMPHP_SEL, MTR1_IV_CMPHP_MUX);
ASysCtl_selectCMPLPMux(MTR1_IV_CMPLP_SEL, MTR1_IV_CMPLP_MUX);
ASysCtl_selectCMPHPMux(MTR1_IW_CMPHP_SEL, MTR1_IW_CMPHP_MUX);
ASysCtl_selectCMPLPMux(MTR1_IW_CMPLP_SEL, MTR1_IW_CMPLP_MUX);
//----- U Phase ------------------------------------------------------------
// Enable CMPSS and configure the negative input signal to come from the DAC
CMPSS_enableModule(obj->cmpssHandle[0]);
// NEG signal from DAC for COMP-H
CMPSS_configHighComparator(obj->cmpssHandle[0], CMPSS_INSRC_DAC);
// NEG signal from DAC for COMP-L
CMPSS_configLowComparator(obj->cmpssHandle[0], CMPSS_INSRC_DAC);
// Configure the output signals. Both CTRIPH and CTRIPOUTH will be fed by
// the asynchronous comparator output.
// Dig filter output ==> CTRIPH, Dig filter output ==> CTRIPOUTH
CMPSS_configOutputsHigh(obj->cmpssHandle[0],
CMPSS_TRIP_FILTER |
CMPSS_TRIPOUT_FILTER);
// Dig filter output ==> CTRIPL, Dig filter output ==> CTRIPOUTL
CMPSS_configOutputsLow(obj->cmpssHandle[0],
CMPSS_TRIP_FILTER |
CMPSS_TRIPOUT_FILTER |
CMPSS_INV_INVERTED);
// Configure digital filter. For this example, the maxiumum values will be
// used for the clock prescale, sample window size, and threshold.
CMPSS_configFilterHigh(obj->cmpssHandle[0], 32, 32, 10);
CMPSS_initFilterHigh(obj->cmpssHandle[0]);
// Initialize the filter logic and start filtering
CMPSS_configFilterLow(obj->cmpssHandle[0], 32, 32, 10);
CMPSS_initFilterLow(obj->cmpssHandle[0]);
// Set up COMPHYSCTL register
// COMP hysteresis set to 2x typical value
CMPSS_setHysteresis(obj->cmpssHandle[0], 1);
// Use VDDA as the reference for the DAC and set DAC value to midpoint for
// arbitrary reference
CMPSS_configDAC(obj->cmpssHandle[0],
CMPSS_DACVAL_SYSCLK | CMPSS_DACSRC_SHDW);
// Set DAC-H to allowed MAX +ve current
CMPSS_setDACValueHigh(obj->cmpssHandle[0], cmpsaDACH);
// Set DAC-L to allowed MAX -ve current
CMPSS_setDACValueLow(obj->cmpssHandle[0], cmpsaDACL);
// Clear any high comparator digital filter output latch
CMPSS_clearFilterLatchHigh(obj->cmpssHandle[0]);
// Clear any low comparator digital filter output latch
CMPSS_clearFilterLatchLow(obj->cmpssHandle[0]);
//---------------- V pHase -------------------------------------------------
// Enable CMPSS and configure the negative input signal to come from the DAC
CMPSS_enableModule(obj->cmpssHandle[1]);
// NEG signal from DAC for COMP-H
CMPSS_configHighComparator(obj->cmpssHandle[1], CMPSS_INSRC_DAC);
// NEG signal from DAC for COMP-L
CMPSS_configLowComparator(obj->cmpssHandle[1], CMPSS_INSRC_DAC);
// Configure the output signals. Both CTRIPH and CTRIPOUTH will be fed by
// the asynchronous comparator output.
// Dig filter output ==> CTRIPH, Dig filter output ==> CTRIPOUTH
CMPSS_configOutputsHigh(obj->cmpssHandle[1],
CMPSS_TRIP_FILTER |
CMPSS_TRIPOUT_FILTER);
// Dig filter output ==> CTRIPL, Dig filter output ==> CTRIPOUTL
CMPSS_configOutputsLow(obj->cmpssHandle[1],
CMPSS_TRIP_FILTER |
CMPSS_TRIPOUT_FILTER |
CMPSS_INV_INVERTED);
// Configure digital filter. For this example, the maxiumum values will be
// used for the clock prescale, sample window size, and threshold.
CMPSS_configFilterHigh(obj->cmpssHandle[1], 32, 32, 10);
CMPSS_initFilterHigh(obj->cmpssHandle[1]);
// Initialize the filter logic and start filtering
CMPSS_configFilterLow(obj->cmpssHandle[1], 32, 32, 10);
CMPSS_initFilterLow(obj->cmpssHandle[1]);
// Set up COMPHYSCTL register
// COMP hysteresis set to 2x typical value
CMPSS_setHysteresis(obj->cmpssHandle[1], 1);
// Use VDDA as the reference for the DAC and set DAC value to midpoint for
// arbitrary reference
CMPSS_configDAC(obj->cmpssHandle[1],
CMPSS_DACVAL_SYSCLK | CMPSS_DACSRC_SHDW);
// Set DAC-H to allowed MAX +ve current
CMPSS_setDACValueHigh(obj->cmpssHandle[1], cmpsaDACH);
// Set DAC-L to allowed MAX -ve current
CMPSS_setDACValueLow(obj->cmpssHandle[1], cmpsaDACL);
// Clear any high comparator digital filter output latch
CMPSS_clearFilterLatchHigh(obj->cmpssHandle[1]);
// Clear any low comparator digital filter output latch
CMPSS_clearFilterLatchLow(obj->cmpssHandle[1]);
//---------------- W Phase -------------------------------------------------
// Enable CMPSS and configure the negative input signal to come from the DAC
CMPSS_enableModule(obj->cmpssHandle[2]);
// NEG signal from DAC for COMP-H
CMPSS_configHighComparator(obj->cmpssHandle[2], CMPSS_INSRC_DAC);
// NEG signal from DAC for COMP-L
CMPSS_configLowComparator(obj->cmpssHandle[2], CMPSS_INSRC_DAC);
// Configure the output signals. Both CTRIPH and CTRIPOUTH will be fed by
// the asynchronous comparator output.
// Dig filter output ==> CTRIPH, Dig filter output ==> CTRIPOUTH
CMPSS_configOutputsHigh(obj->cmpssHandle[2],
CMPSS_TRIP_FILTER |
CMPSS_TRIPOUT_FILTER);
// Dig filter output ==> CTRIPL, Dig filter output ==> CTRIPOUTL
CMPSS_configOutputsLow(obj->cmpssHandle[2],
CMPSS_TRIP_FILTER |
CMPSS_TRIPOUT_FILTER |
CMPSS_INV_INVERTED);
// Configure digital filter. For this example, the maxiumum values will be
// used for the clock prescale, sample window size, and threshold.
CMPSS_configFilterHigh(obj->cmpssHandle[2], 32, 32, 10);
CMPSS_initFilterHigh(obj->cmpssHandle[2]);
// Initialize the filter logic and start filtering
CMPSS_configFilterLow(obj->cmpssHandle[2], 32, 32, 10);
CMPSS_initFilterLow(obj->cmpssHandle[2]);
// Set up COMPHYSCTL register
// COMP hysteresis set to 2x typical value
CMPSS_setHysteresis(obj->cmpssHandle[2], 1);
// Use VDDA as the reference for the DAC and set DAC value to midpoint for
// arbitrary reference
CMPSS_configDAC(obj->cmpssHandle[2],
CMPSS_DACVAL_SYSCLK | CMPSS_DACSRC_SHDW);
// Set DAC-H to allowed MAX +ve current
CMPSS_setDACValueHigh(obj->cmpssHandle[2], cmpsaDACH);
// Set DAC-L to allowed MAX -ve current
CMPSS_setDACValueLow(obj->cmpssHandle[2], cmpsaDACL);
// Clear any high comparator digital filter output latch
CMPSS_clearFilterLatchHigh(obj->cmpssHandle[2]);
// Clear any low comparator digital filter output latch
CMPSS_clearFilterLatchLow(obj->cmpssHandle[2]);
// HVMTRPFC_REV1P1
#endif // !HVMTRPFC_REV1P1
#endif // !(MOTOR1_ISBLDC || MOTOR1_DCLINKSS)
return;
} // end of HAL_setupCMPSSs() function