etpwmStartTBCLK()用于启用TBCLKSYNC。设置TBCLKSYNC时,所有ePWM时基时钟都在TBCLK的上升沿对齐的情况下启动。当TBCLKSYNC为0时,所有ePWM模块的时基时钟都将停止。
也就是说,目前确实没有办法单独控制
您可以看一下说明
20.2.3 Analog-to-Digital Converter Core
The analog conversion range is determined by the reference voltages: ADREFHI and ADREFLO. ADREFHI is the top reference voltage and is the maximum analog voltage that can be converted.
各位好,我想问下
1、如下图为评估板的原理图,这里ADC参考电压这里加的电阻是干什么用的。我们自己的板子 加了这个电阻,参考电压就达不到3.3V了。
2、ADC同样的配置,加这个电阻和不加这个电阻真实的采样率不一样是怎么回事,按道理说这个只是影响参考电压,为什么采样率也被影响了。