Other Parts Discussed in Thread: MSP430F4152, UNIFLASH, MSP430F5529
利用 information memory 保存数据;原始数据通过编程器下载进去,程序如下:
#pragma location = 0x1040
__root const uint8_t INFO_1[64] = {。。。。。}
现在发现一部分MCU上电读出来的数据有FF FE之类的乱码,上电只读没有写操作。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: MSP430F4152, UNIFLASH, MSP430F5529
利用 information memory 保存数据;原始数据通过编程器下载进去,程序如下:
#pragma location = 0x1040
__root const uint8_t INFO_1[64] = {。。。。。}
现在发现一部分MCU上电读出来的数据有FF FE之类的乱码,上电只读没有写操作。
以下是相关的测试代码以及实验结果
测试代码
/* --COPYRIGHT--,BSD_EX
* Copyright (c) 2012, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*******************************************************************************
*
* MSP430 CODE EXAMPLE DISCLAIMER
*
* MSP430 code examples are self-contained low-level programs that typically
* demonstrate a single peripheral function or device feature in a highly
* concise manner. For this the code may rely on the device's power-on default
* register values and settings such as the clock configuration and care must
* be taken when combining code from several examples to avoid potential side
* effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware
* for an API functional library-approach to peripheral configuration.
*
* --/COPYRIGHT--*/
//******************************************************************************
// MSP430F552x Demo - Flash In-System Programming w/ Long-Word write at 0x1800
//
// Description: This program first erases flash seg D, then it writes a 32-bit
// value to memory location 0x1800 using long-word write mode. Long-word write
// provides faster write than byte/word mode.
// ACLK = REFO = 32kHz, MCLK = SMCLK = default DCO 1048576Hz
//
// MSP430x552x
// -----------------
// /|\| XIN|-
// | | |
// --|RST XOUT|-
// | |
//
//
// Bhargavi Nisarga
// Texas Instruments Inc.
// April 2009
// Built with CCSv4 and IAR Embedded Workbench Version: 4.21
//******************************************************************************
#include <msp430.h>
int main(void)
{
unsigned long * Flash_ptrD; // Initialize Flash pointer Seg D
unsigned long value;
WDTCTL = WDTPW+WDTHOLD; // Stop WDT
Flash_ptrD = (unsigned long *) 0x1800; // Initialize Flash pointer
value = 0x12345678; // Initialize Value
FCTL3 = FWKEY; // Clear Lock bit
FCTL1 = FWKEY+ERASE; // Set Erase bit
*Flash_ptrD = 0; // Dummy write to erase Flash seg
FCTL1 = FWKEY+BLKWRT; // Enable long-word write
*Flash_ptrD = value; // Write to Flash
FCTL1 = FWKEY; // Clear WRT bit
FCTL3 = FWKEY+LOCK; // Set LOCK bit
while(1); // Loop forever, SET BREAKPOINT HERE
}
测试过程
1 在CCS内新建工程,写入代码,编译成功后连接开发板调试
可以发现程序运行后,0x1800处已经成功写入数据
2 而后板子断电,而后重新连接电脑上的uniflash来读memory,数据依然存在