Other Parts Discussed in Thread: MSP430F2274
这款单片机的ADC模块,选择ADC10的通道时候,手册里面有一个(VCC-VSS)/2,没看懂是什么意思,求帮忙解答 ,谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: MSP430F2274
这款单片机的ADC模块,选择ADC10的通道时候,手册里面有一个(VCC-VSS)/2,没看懂是什么意思,求帮忙解答 ,谢谢
什么是电源电压一半 说ADC的参考电压吗 还是啥 我想弄明白的是参考电压电一半指的是啥呢
Up to eight external input channels (twelve on MSP430F22xx devices)
这里是指的输入通道,而A12等表示的是输入通道为固定值(VCC - VSS) / 2
看一下下面的例程,会对您有所帮助
/* --COPYRIGHT--,BSD_EX
* Copyright (c) 2012, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*******************************************************************************
*
* MSP430 CODE EXAMPLE DISCLAIMER
*
* MSP430 code examples are self-contained low-level programs that typically
* demonstrate a single peripheral function or device feature in a highly
* concise manner. For this the code may rely on the device's power-on default
* register values and settings such as the clock configuration and care must
* be taken when combining code from several examples to avoid potential side
* effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware
* for an API functional library-approach to peripheral configuration.
*
* --/COPYRIGHT--*/
//******************************************************************************
// MSP430F22x4 Demo - ADC10, Sample A11, Lo_Batt, Set P1.0 if AVcc < 2.3V
//
// Description: A single sample is made on A11 (AVcc/2) with reference to
// internal 1.5V Vref. Software sets ADC10SC to start sample and conversion
// - ADC10SC automatically cleared at EOC. ADC10 internal oscillator times
// sample (16x) and conversion. ADC10BUSY flag is polled for EOC. If A11
// (AVcc/2) < 0311h (1.15V) indicating AVcc is less 2.3V, P1.0 set indicating
// a lo_Batt condition, else reset.
//
// MSP430F22x4
// -----------------
// /|\| XIN|-
// | | |
// --|RST XOUT|-
// | |
// |A11 (AVcc/2) P1.0|-->LED
//
// A. Dannenberg
// Texas Instruments Inc.
// April 2006
// Built with CCE Version: 3.2.0 and IAR Embedded Workbench Version: 3.41A
//******************************************************************************
#include <msp430.h>
int main(void)
{
WDTCTL = WDTPW + WDTHOLD; // Stop WDT
ADC10CTL1 = INCH_11; // AVcc/2
ADC10CTL0 = SREF_1 + ADC10SHT_2 + REFON + ADC10ON;
TACCR0 = 30; // Delay to allow Ref to settle
TACCTL0 |= CCIE; // Compare-mode interrupt
TACTL = TASSEL_2 + MC_1; // TACLK = SMCLK, Up mode
__bis_SR_register(CPUOFF + GIE); // LPM0, TA0_ISR will force exit
TACCTL0 &= ~CCIE; // Disable timer Interrupt
P1DIR |= 0x01; // Set P1.0 to output direction
for (;;)
{
ADC10CTL0 |= ENC + ADC10SC; // Sampling and conversion start
while (ADC10CTL1 & ADC10BUSY); // ADC10BUSY?
if (ADC10MEM < 0x311) // ADC10MEM = A11 > 1.15V?
P1OUT |= 0x01; // Set P1.0 LED on
else
P1OUT &= ~0x01; // Clear P1.0 LED off
}
}
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=TIMERA0_VECTOR
__interrupt void TA0_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(TIMERA0_VECTOR))) TA0_ISR (void)
#else
#error Compiler not supported!
#endif
{
TACTL = 0; // Clear Timer_A control registers
LPM0_EXIT; // Exit LPM0 on return
}