This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这款单片机的ADC模块,选择ADC10的通道时候,手册里面有一个(VCC-VSS)/2,没看懂是什么意思,求帮忙解答 ,谢谢
什么是电源电压一半 说ADC的参考电压吗 还是啥 我想弄明白的是参考电压电一半指的是啥呢
Up to eight external input channels (twelve on MSP430F22xx devices)
这里是指的输入通道,而A12等表示的是输入通道为固定值(VCC - VSS) / 2
看一下下面的例程,会对您有所帮助
/* --COPYRIGHT--,BSD_EX * Copyright (c) 2012, Texas Instruments Incorporated * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * ******************************************************************************* * * MSP430 CODE EXAMPLE DISCLAIMER * * MSP430 code examples are self-contained low-level programs that typically * demonstrate a single peripheral function or device feature in a highly * concise manner. For this the code may rely on the device's power-on default * register values and settings such as the clock configuration and care must * be taken when combining code from several examples to avoid potential side * effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware * for an API functional library-approach to peripheral configuration. * * --/COPYRIGHT--*/ //****************************************************************************** // MSP430F22x4 Demo - ADC10, Sample A11, Lo_Batt, Set P1.0 if AVcc < 2.3V // // Description: A single sample is made on A11 (AVcc/2) with reference to // internal 1.5V Vref. Software sets ADC10SC to start sample and conversion // - ADC10SC automatically cleared at EOC. ADC10 internal oscillator times // sample (16x) and conversion. ADC10BUSY flag is polled for EOC. If A11 // (AVcc/2) < 0311h (1.15V) indicating AVcc is less 2.3V, P1.0 set indicating // a lo_Batt condition, else reset. // // MSP430F22x4 // ----------------- // /|\| XIN|- // | | | // --|RST XOUT|- // | | // |A11 (AVcc/2) P1.0|-->LED // // A. Dannenberg // Texas Instruments Inc. // April 2006 // Built with CCE Version: 3.2.0 and IAR Embedded Workbench Version: 3.41A //****************************************************************************** #include <msp430.h> int main(void) { WDTCTL = WDTPW + WDTHOLD; // Stop WDT ADC10CTL1 = INCH_11; // AVcc/2 ADC10CTL0 = SREF_1 + ADC10SHT_2 + REFON + ADC10ON; TACCR0 = 30; // Delay to allow Ref to settle TACCTL0 |= CCIE; // Compare-mode interrupt TACTL = TASSEL_2 + MC_1; // TACLK = SMCLK, Up mode __bis_SR_register(CPUOFF + GIE); // LPM0, TA0_ISR will force exit TACCTL0 &= ~CCIE; // Disable timer Interrupt P1DIR |= 0x01; // Set P1.0 to output direction for (;;) { ADC10CTL0 |= ENC + ADC10SC; // Sampling and conversion start while (ADC10CTL1 & ADC10BUSY); // ADC10BUSY? if (ADC10MEM < 0x311) // ADC10MEM = A11 > 1.15V? P1OUT |= 0x01; // Set P1.0 LED on else P1OUT &= ~0x01; // Clear P1.0 LED off } } #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__) #pragma vector=TIMERA0_VECTOR __interrupt void TA0_ISR(void) #elif defined(__GNUC__) void __attribute__ ((interrupt(TIMERA0_VECTOR))) TA0_ISR (void) #else #error Compiler not supported! #endif { TACTL = 0; // Clear Timer_A control registers LPM0_EXIT; // Exit LPM0 on return }