This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5529: 上电无法复位,Reset短接地也无法完成复位

Part Number: MSP430F5529


一、现象:

1、目前生产中一批板子陆续出现上电无法完成复位现象,短接RST引脚也无法复位;

二、测试

1、取异常板子,下载最简单的程序(主程序中只执行关狗+IO置低电平+while(1)操作),在使用IAR下载完程序并执行后能够正常开机,但是之后短接RST后再次死机,程序无法执行到IO置低电平位置;

2、MSP430F5529  3.3V供电正常,上电1ms内上升至3.3V,过程无回落,复位电路采用100K+0.1uF组合;

3、基于上述程序,在对芯片的核心电压Vcore量取中发现,Vcore电压在上电瞬间变成1.4V左右,保持约30-50ms后在100us内升至1.92V左右,这样情况下板子上电无法执行第一行程序;且短接RST过程中Vcore电压降至1.4V,不在短接RST后又升至1.92V,芯片还是无法执行第一行程序,程序中并没有修改Vcore电压的配置;Vcore电压在user's Guide中明确写该电压上电后处于最低值。