This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR5043: 调试超声波传感器,开始捕捉信号时,就一直卡在了 Wait until USS module is in READY state,请问怎么检查了

Part Number: MSP430FR5043


__interrupt void USSLIB_HAL_TIMER_RXEN_INT(void)
{
switch(__even_in_range(HARDWAREWREG16(USSSWLIB_HAL_RXEN_TIMER_BASE_ADDRESS + OFS_TAxIV),
TAIV__TAIFG))
{
    case TAIV__NONE: break; // No interrupt
    case TAIV__TACCR1: // CCR1, Enables RXEN
         // Enable RxEN, RxEN will be turned Off after USS acquisition
         USSSWLIB_HAL_AFE_RXEN_PORT |= (USSSWLIB_HAL_AFE_RXEN_PIN);
        // Disable Timer
         HARDWAREWREG16(USSSWLIB_HAL_RXEN_TIMER_BASE_ADDRESS + OFS_TAxCTL) &= ~(MC_3 | TAIFG);
         break;
     case TAIV__TACCR2: // CCR2, start ASQ, restart timer to trigger RxEN
          // Wait until USS module is in READY state
          while((UUPSCTL & UPSTATE_3) != UPSTATE_3);