This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
之前没有找到问题设备,现在找到了,但运行了图里面的代码,RTC_B没有恢复正常,RTC_B读取数据比较乱,产生的中断也比较乱,不是1秒产生一次,读取的三个寄存器数据如下:BAKMEM0 = 0xf7bc RTCCTL01 = 0xb007 RTCCTL2 = 0x0081
你好,您是否遵循以下应用说明来确保正确更新相应的寄存器,以确保在电源中断时 RTC_B 能够正确运行?具体第 3 节:www.ti.com/lit/slaa665
您的备用电池电路是什么样的?是否有可能在过渡期间被耗尽?
你好,参考下工程师的回复:
我在上面链接的应用笔记中概述了一些步骤,以确保 RTC_B 在断电时保持不变,并在数据损坏时正确处理。该应用程序说明还包括演示代码,展示了正确的处理方式。
话虽如此,停电 10 天已经是相当长的时间了。他们的备用电池是否有足够的电力储备来处理这个问题?电源恢复后有办法充电吗?或者备份耗尽后是否需要更换?这些是您应该问客户的问题。话虽这么说,我只是看了他们的原理图,他们没有备用电池。他们只是将 VBAT 与小盘股 VCC 挂钩。因此,一旦失去主电源(VCC),该电容就会很快放电。所以是的,我预计这里会出现损坏,因为它们没有 RTC_B 的备用电源。
参考下工程师的回复:
A BOR would clear all of the RTC data. I would start with our code example to make sure everything is working properly, then do a delta of your solution to the code example to see what's going on.
Also, make sure you are handling the LOCKBAK bit correctly when doing your changes.
参考下下面的回复:
There is no command, but you cna program the device to go into the different LPM modes. Most interrupts wakeup the device from all power modes, with the exception of the LPMx.5 modes. They can only be woken up by RTC (LPM3.5 only), power sequence, RST, or a specific I/O.
参考下下面的回复:
I think you maybe running into the RTC16 errata here due to how the power scheme is this design. Some of the behavior you are describing is similar to that errata. The customer's hardware design would have to account for the errata workaround to prevent this.
参考下下面的回复:
LPM4.5 disables and power gates the RTC. You would need to utilize LPM3.5 on those devices. Also,again the hardware power scheme is not conducive to the application. The customer needs a seperate power source of some type in order to keep the RTC running when they lose main power. Also to avoid the errata RTC16, they need to ensure that power source behaves as the workaround describes.