刚刚学习msp430F5529但是看的教程什么的都是F149的,现在弄一个模块。一编译一堆错误~~~晕死。应该是f149寄存器的名字和f5529的不一样,有没有资料解释一下他们的关系。
void main( void ) { unsigned char i ; WDTCTL= WDTPW + WDTHOLD; //关闭看门狗 BCSCTL1 &= ~XT2OFF; //基础时钟控制寄存器BCSCTL1的第7位置0,使XT2启动 do { IFG1 &= ~OFIFG; for(i= 0xff; i>0; i--); } while ((IFG1 & OFIFG)!=0); BCSCTL2 |= SELS; TACTL=TACLR+ID0+ID1+TASSEL1; //SMCLK为时钟源,清TAR CCR0 =0xffff; CCTL0 = CCIE; init(); P2SEL = 0X00; P2DIR = 0XFE; P2OUT = 0X00; P2IE=0X01; P2IES=0X00; P2IFG=0; _EINT(); DispNChar(1,0,12,tab1); while(1) { if(flag==0) {P2OUT |= SEG2; delay_ms(12); P2OUT &= ~SEG2; delay_ms(12); } Disp1Char(1,1,tab[temp/1000]); Disp1Char(2,1,'.'); Disp1Char(3,1,tab[temp/100%10]); Disp1Char(4,1,tab[temp/10%10]); Disp1Char(5,1,tab[temp%10]); Disp1Char(6,1,'M'); } } #pragma vector =PORT2_VECTOR //p2中断服务 __interrupt void anjian(void) { if(UG==1) { TACTL |=MC0; //停止模式 TAR=0; _DINT(); P2OUT=0X00; P2IES=0X01; //P2.0 下降沿触发 P2IE=0; //不允许中断 P2IFG=0; //没有中断 P2IE=1; //允许中断 UG=0; _EINT(); flag=1; } else { TACTL &= ~MC0; temp=TAR; //读取数据 temp=temp*0.172; UG=1; P2IES=0X00; P2IE=0; P2IFG=0; P2IE=1; flag=0; } }