• MSP430FR6043: 关于

    Part Number: MSP430FR6043

     1.GUI中可以得到顺逆和逆流的波形,但是互相关的波形该如何得到?

    2保存ADC capture后的文档里给出了DTOF,Abs TOF,Dns TOF的数据是已经经过互相关和插值计算的到的数据吗?

  • EVM430-FR6043: EVM430-FR6043内的程序移植到MSP430FR5043

    Part Number: EVM430-FR6043
    Other Parts Discussed in Thread: MSP430FR6043, , MSP430FR5043

    Hi,我目前是使用EVM430-FR6043与上位机进行开发,但是在项目实际中使用的是MSP430FR5043的单片机,所以需要将MSP430FR6043的程序移植到MSP430FR5043单片机中,通过修改Variant中的芯片选型,将其改为MSP430FR5043后,其链接器文件也修改为lnk_msp430fr5043…

  • MSP430FR6043: How the USS library algorithmically calculates gas TOF times

    Part Number: MSP430FR6043

    hi,

        I would like to know how to calculate the gas TOF time from the ADC data, the code for this is in the lib library and I can't view it, do you have a document that describes the implementation of the algorithm through the…

  • EVM430-FR6043: Ultrasonic Design Center配置的各项参数

    Part Number: EVM430-FR6043

    我使用这块评估板,往其中下载了SDK中的Gas_Demo,然后在Ultrasonic Design Center中配置各项参数,有以下几个问题

    1:我想知道这些配置的参数都对应在这个Demo中的哪些代码中。

    2:关于ADC部分,我没有在代码中找到关于ADC的相关代码。

    3:关于ABS_TOF,没有找到ABS_TOF的参数,是否是需要用(ABS_UPS+ABS_DNS)/2来计算?

    希望能尽快回复,谢谢!

  • EVM430-FR6043: 开发板的LCD模式是如何开启的

    Part Number: EVM430-FR6043
    Other Parts Discussed in Thread: MSP430FR6043

       在开发板上并没有找到UP导航按钮 但时候有时候LCD会自己亮起并显示

  • MSP430FR6043: 固件烧写熔断保护

    Part Number: MSP430FR6043
    Other Parts Discussed in Thread: UNIFLASH, MSP-FET

    请问MSP430FR6043是否支持固件烧写后熔断保护?即不支持程序的读取和再烧写。

  • EVM430-FR6043: 关于液位计的设计

    Part Number: EVM430-FR6043
    Other Parts Discussed in Thread: UNIFLASH, MSP430FR6043

    用此开发板设计一个液位计,按照所给定的技术文档连接换能器后,是否需要将开发板内部的固件以及MSP430-FR6043单片机中的程序换为Ultrasonic WaterFR604X和官方给出的Water Demo?

  • MSP430FR6043: 什么影响气表和水表的采样点数

    Part Number: MSP430FR6043

       你好,MSP430FR6043为什么气表工程是500个点,水表工程是160个点,什么影响了他们的采样点数

  • MSP430FR6043: MSP430FR6043与MSP430FR60431的区别

    Part Number: MSP430FR6043

    问个问题,MSP430FR6043与MSP430FR60431的区别是什么,除了支持的BSL接口分别是UART和IIC,这两个型号之间还有其他区别吗?

  • MSP430FR6043: MSP430FR6043飞行时间

    Part Number: MSP430FR6043

    MSP430FR6043用于超声波测距,TOF时间是否有限制,20ms以内可以吗?

  • MSP430FR6043: CCS20索引问题

    Part Number: MSP430FR6043

    当我使用最新版本CCS20.0.1.4__1.6.1打开UltrasonicGasFR6043_02_30_00_01例程,编译成功,但尝试使用右键跳转到函数定义处,发现无法成功跳转,且搜索函数名称,也无法索引出函数所在位置,这是为什么呢?

  • MSP430FR6043: MSP-FET固件更新失败,程序下载调试失败

    Part Number: MSP430FR6043
    Other Parts Discussed in Thread: MSP-FET, MSP-TS430PN80C

    不知道为什么,当我首次尝试使用MSP-FET连接MSP-TS430PN80C开发板时,CCS提示需要更新固件,但当我点击Update后,固件并未更新成功,且当我尝试直接烧写或debug例程时,也无法成功,这是为什么呢?因为不清楚开发板的外部供电电压要求,我使用JTAG接口直接供电。

  • MSP430FR6043: uss上位机

    Part Number: MSP430FR6043

    你好,我对贵公司的上位机的参数有些疑问,能解答一下吗?比如     我看Ultrasonic Sensing  Design  Center  文档有部分说明,但是不是很全面

  • MSP430FR6043: 使用最新版本的CCS编译例程,如何指定生成烧写文件的类型和路径

    Part Number: MSP430FR6043
    Other Parts Discussed in Thread: SYSCONFIG

    如题,使用最新版本的CCS20.0.1.4__1.6.1编译例程UltrasonicGasFR6043_02_30_00_01,如何指定生成烧写文件的类型和路径?

  • MSP430FR6043: msp430fr6043的时钟替换

    Part Number: MSP430FR6043

    你好,如果我把MSPFR6043的Y1的晶振变为24M,我的gas_demo工程应该如果配置

  • MSP430FR6043: UltrasonicGasFR6043工程导入失败

    Part Number: MSP430FR6043

    当我使用CCS10.3.1.00003 导入UltrasonicGasFR6043_02_30_00_01例程时,提示如下错误:See details below...
        Import failed for project 'UltrasonicGasFR6043_02_30_00_01' because its meta-data cannot be interpreted. Please contact support.

    而…

  • MSP430FR6043: 支持的换能器频率范围

    Part Number: MSP430FR6043

    问一下,MSP430FR6043支持的换能器频率范围是多少?

  • EVM430-FR6043: USS调试接口IIC使用问题!

    Part Number: EVM430-FR6043
    Other Parts Discussed in Thread: MSP430FR6043

    硬件指南里写到J1 provides a connection between the MSP430FR6043 MCU and the high-speed USB HID interface. To enable I 2C, put jumpers on the J1 COMM_SDA, COMM_SCL, and COMM_IRQ pins (see…

  • MSP430FR6043: EVM连接换能器方案与实际应用换能器通道连接方案

    Part Number: MSP430FR6043
    Other Parts Discussed in Thread: EVM430-FR6043,

    您好!

    请问EVM430-FR6043展示连接换能器,由CH0通过电子开关切换驱动两个换能器,实际应用中是否可以CH0、CH1分别驱动上行、下行的换能器发送?例程代码有提供吗?

  • MSP430FR6043: 在IAR软件里导入USS SW 库中的项目文件_USSSWLib_template_example编译失败

    Part Number: MSP430FR6043

    Fatal Error[e72]: Segment RAM-THRILl must be defined in a segment definition option (-Z, -b or -P) 该怎么解决

  • MSP430FR6043: 水的官方应用用例

    Part Number: MSP430FR6043
    Other Parts Discussed in Thread: MSP430FR6047,

    你好,官网有MSP430FR6043的水测试用例吗?只有MSP430FR6047的吗?MSP430FR6043的我需要如何修改固件

  • MSP430FR6043: MSP430FR6043如何支持水的测试

    Part Number: MSP430FR6043
    Other Parts Discussed in Thread: MSP430FR6047,

    你好,如果我要作为水表固件改如何修改?我看MSP430FR6043只有gas的软件工程,MSP430FR6047才有water的软件工程,MSP430FR6043能移植water的软件工程吗?如果能,能给出详细的修改点吗?MSP430FR6047的water工程如何移植到MSP430FR6043上面,或者MSP430FR6043的gas工程如何修改为能测试水…

  • MSP430FR6043: 水表测试的问题

    Part Number: MSP430FR6043
    Other Parts Discussed in Thread: MSP430FR6047,

    你好,如果我要作为水表固件改如何修改?我看MSP430FR6043只有gas的软件工程,MSP430FR6047才有water的软件工程,MSP430FR6043能移植water的软件工程吗?如果能,能给出详细的修改点吗?

    TRANSLATE with x
    English
    Arabic Hebrew Polish
    Bulgari…
  • MSP430FR6043: 如果在实际应用中传播时间Tprop大概是5ms左右,远远大于70微妙 。那么USS 设计中心还能用吗,如果还能用,应该怎么用?

    Part Number: MSP430FR6043

    如果在实际应用中传播时间Tprop大概是5ms左右,远远大于70微妙 。那么USS 设计中心还能用吗,如果还能用,应该怎么用?

  • MSP430FR6043: MSP430FR6043晶振输出问题

    Part Number: MSP430FR6043
    Other Parts Discussed in Thread: MSP430FR6047

    你好,如何把内部陶瓷晶振输出到gpio脚上,应该如何配置芯片

1 2 3 4 5 »