• MSP430FR6047: 一个芯片测量两个流量计

    Part Number: MSP430FR6047

    我想通过一个MSP430FR6047测量两个流量计部件,中间使用模拟开关来切换,除了在程序中添加模拟开关的控制以外,其他算法部分需要做修改吗

  • MSP430FR6047: 串口数据被篡改、通道发送问题

    Part Number: MSP430FR6047

    项目进度比较急,麻烦TI官方提供帮助。目前我发现我在使用P8.2和P8.3引脚作为串口通信时,所接受到的数据不对,经过我的排查,已经排除波特率等配置相关问题,后将问题锁定到是由于开启了低功耗导致,当我屏蔽了低功耗后,数据就正常了。在这里有一个新的问题,总所周知,超声波流量计需要探头A发送脉冲,B作为接收得到一个数据,探头B发送脉冲,A作为接收得到另一个数据,但在USS库的代码中,我并未找到什么时候是控制A发送脉冲,什么时候控制B发送脉冲,我需要在发送脉冲时做一些处理使用…

  • MSP430FR6047: 我想在不同通道发送脉冲时进行一些IO口操作

    Part Number: MSP430FR6047

    您好,我想在CH0发送脉冲时将一个IO口拉低,CH1发送脉冲时将此IO口拉高,请问如何实现,控制CH0和CH1发送脉冲的命令在哪,我取消了低功耗的状态,使用USS_startUltrasonicMeasurement进行测量的。

  • EVM430-FR6043: Ultrasonic Design Center配置的各项参数

    Part Number: EVM430-FR6043

    我使用这块评估板,往其中下载了SDK中的Gas_Demo,然后在Ultrasonic Design Center中配置各项参数,有以下几个问题

    1:我想知道这些配置的参数都对应在这个Demo中的哪些代码中。

    2:关于ADC部分,我没有在代码中找到关于ADC的相关代码。

    3:关于ABS_TOF,没有找到ABS_TOF的参数,是否是需要用(ABS_UPS+ABS_DNS)/2来计算?

    希望能尽快回复,谢谢!

  • MSP430FR6047: MSP430FR6047编译过程报错

    Part Number: MSP430FR6047

    请问这个报错是不是需要更新 stdlib 库吗? 还有单独下载这个库需要哪里下载?谢谢!

  • MSP430FR6047: 串口数据被篡改

    Part Number: MSP430FR6047

    您好!我在使用MSP430FR6047的水表评估板时遇到了一个问题,使用的是DEMO软件,我在其中添加了P8.2和P8.3引脚作为串口输出,在仅执行串口收发数据是正常的,在我将水表计量相关的函数打开后,接收的数据和就不正常了,请问是APP的某个地方会影响串口收发吗?

  • MSP430FR6047: 关于例程中的计算结果

    Part Number: MSP430FR6047
    Other Parts Discussed in Thread: EVM430-FR6047

    您好:

         我在EVM430-FR6047开发板的官网例程中看到,测量的时差和传输时间都是函数计算出,放到关于结果的一个结构体变量(alg_results_float)中,用户可以从这个机构体取出结果并使用,那么我想问的是,这个结构体中,时差的计算是由正逆程的传输时间相减得到的吗?

    期待您的解答!

    TRANSLATE with x
    Englis…
  • MSP430FR5043: 我想使用MSP430FR5043芯片制作一个水表

    Part Number: MSP430FR5043

    但是在制作过程中我发现飞行时间会偶发的跳到0.8ns,但是下一个点又自动恢复,我想知道是我配置的问题吗

  • MSP430FR6043: 水的官方应用用例

    Part Number: MSP430FR6043
    Other Parts Discussed in Thread: MSP430FR6047,

    你好,官网有MSP430FR6043的水测试用例吗?只有MSP430FR6047的吗?MSP430FR6043的我需要如何修改固件

  • MSP430FR6043: MSP430FR6043如何支持水的测试

    Part Number: MSP430FR6043
    Other Parts Discussed in Thread: MSP430FR6047,

    你好,如果我要作为水表固件改如何修改?我看MSP430FR6043只有gas的软件工程,MSP430FR6047才有water的软件工程,MSP430FR6043能移植water的软件工程吗?如果能,能给出详细的修改点吗?MSP430FR6047的water工程如何移植到MSP430FR6043上面,或者MSP430FR6043的gas工程如何修改为能测试水…

  • MSP430FR6043: 水表测试的问题

    Part Number: MSP430FR6043
    Other Parts Discussed in Thread: MSP430FR6047,

    你好,如果我要作为水表固件改如何修改?我看MSP430FR6043只有gas的软件工程,MSP430FR6047才有water的软件工程,MSP430FR6043能移植water的软件工程吗?如果能,能给出详细的修改点吗?

    TRANSLATE with x
    English
    Arabic Hebrew Polish
    Bulgari…
  • MSP430FR6043: MSP430FR6043晶振输出问题

    Part Number: MSP430FR6043
    Other Parts Discussed in Thread: MSP430FR6047

    你好,如何把内部陶瓷晶振输出到gpio脚上,应该如何配置芯片

  • EVM430-FR6047: Urgency questions as below need to help

    Part Number: EVM430-FR6047
    Other Parts Discussed in Thread: MSP430FR6047

    Other Parts Discussed in Thread: MSP430FR6047


    Can you help us to ask TI experts,Consult technical questions
    We are now using the MSP430FR6047 Ultrasonic Sensing Evaluation Module to…

  • EVM430-FR6047: Consult technical questions about ultrasonic flow metering calibration

    Part Number: EVM430-FR6047
    Other Parts Discussed in Thread: MSP430FR6047


    Can you help us to ask TI experts,Consult technical questions
    We are now using the MSP430FR6047 Ultrasonic Sensing Evaluation Module to design an ultrasonic flow meter, asking questions…

  • MSP430FR6043: 。

    Part Number: MSP430FR6043

    超声波传感设计中心图形用户界面为什么安装成功后突然退出了  再点开的时候就显示无法解析给定配置

  • MSP430FR6043: 更多容量的芯片

    Part Number: MSP430FR6043

    这款芯片的RAM是4K,有更大的内存的芯片吗?

  • MSP430F5529: 在哪里可以取得io430.h和io430f5529.h文件?

    Part Number: MSP430F5529

    在网上下载了一个使用msp430f5529的关于RS485的MODBUS RTU协议的例程,例程里含有#include "io430.h"和#include "io430f5529.h"。运行程序,提示问题显示找不到这两个文件,CCS IDE版本是ccs 11.0.0。在msp430.h文件中也找不到该文件。

  • EVM430-FR6047: MSP 低功耗微控制器论坛

    Part Number: EVM430-FR6047
    Other Parts Discussed in Thread: UNIFLASH

    Hi,

    I use the EVM430-FR6047 connenct to the PC, but it shows there are two port connected(show below), the location info is the same.  I have trasfer to another PC, still two ports.

  • MSP430FR6047: 驱动频率是否可以设置到200KHz

    Part Number: MSP430FR6047

    使用USS软件设置驱动频率只能到780KHz,芯片是否可以产生200Khz的频率呢。

  • MSP430FR6047: MCLK提高到16MHz后,不能与设计中心正常通讯

    Part Number: MSP430FR6047
    Other Parts Discussed in Thread: EVM430-FR6047,

    在EVM430-FR6047开发板中,我将MSP430fr6047芯片的主频MCLK修改为16MHz后,板子不能与设计中心正常通讯。我选择的通讯接口是I2C接口。我希望将主频提高以提高运算速率,但是又能够保持与设计中心正常通讯,有什么办法能做到吗?

  • MSP430FR6047: 不同材质的管道中液体流量的测量问题

    Part Number: MSP430FR6047

    你好,目前我在进行流量计对不同材质管道的适应性检测,所采用的换能器安装方式为“V”型安装,如下图所示:

    当装置安装在PVC管道上时,在上位机软件上貌似可以看到两个特征明显的波瓣,当Gap between pulse start and ADC capture 此参数为40时,波形图如下:

    Gap between pulse start and ADC capture 此参数为80时,波形图如下:

    当Gap between…

  • MSP430FR6047: 波瓣找寻错误后,超声波部分如何暂停或者断开

    Part Number: MSP430FR6047

    您好!

    我使用MSP430FR6047进行了水计量相关的开发,现在遇到一个问题:

    超声波寻找波瓣时,不定时的出现波瓣找寻错误(前一个或者后一个),从而导致dtof增大/减小一个波瓣的数值,大概为±17500000。

    找寻错误后,一般会持续错误,直到流量归零,或者物理断开换能器。也有几率一段时间后自动恢复正常。

    该问题在温度50℃往上尤为明显。

    基于我自己的流道,当前的USS_ALG_RATIO_OF_TRACK_LOBE  0.1…

  • MSP430FR6043: MSP430FR6043和MSP430FR6047的功耗疑问

    Part Number: MSP430FR6043

    您好,看数据手册中测气和测水的功耗,差别感觉很明显,而且有些地方感觉有些不合理,比如,sleep的静态电流为何不同,Data process的电流为何不同?这是为啥

  • MSP430FR6047: 超声波回波信号存在直流偏置

    Part Number: MSP430FR6047

    我又遇到这个问题了,这次我打开了宏USS_APP_DC_OFFSET_CANCELLATION_ENABLE,但是看起来好像没什么效果。还有其他方法可以消除直流偏置吗?

  • MSP430FR6047: RAM不够用,如何变量放置到FRAM

    Part Number: MSP430FR6047

    因为芯片RAM不够用,所以我想把变量放置到FRAM,于是我打开了链接文件中的这个宏定义__USS_RUN_ALG_FROM_RAM__,打开宏定义之后,程序就不能正常运行了。请问是我忽略了什么吗?我该怎么做,才能让程序正常运行?

1 2 3 4 5 »