Part Number: MSPM0G3519
Other Parts Discussed in Thread: SYSCONFIG
MCAN_IR的pea位被置1,产生的仲裁协议错误该如何修复
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSPM0G3519
Other Parts Discussed in Thread: SYSCONFIG
MCAN_IR的pea位被置1,产生的仲裁协议错误该如何修复
void MCAN_BUS_OFF_recovery(void)
{
// 将基地址转换为 MCAN_Regs 结构体指针
volatile MCAN_Regs * const mcan_regs = (MCAN_Regs *)MCAN_BASE_ADDRESS;
// 读取 MCAN_PSR 数据
uint32_t psr_value = mcan_regs->MCANSS.MCAN.MCAN_PSR;
// 提取 BO 位的值
uint8_t bo_bit = (psr_value & MCAN_PSR_BO_MASK) >> MCAN_PSR_BO_OFS;
// 读取 MCAN_CCCR 数据
uint32_t cccr_value = mcan_regs->MCANSS.MCAN.MCAN_CCCR;
// 提取 INIT 位的值
uint8_t init_bit = (cccr_value & MCAN_CCCR_INIT_MASK) >> MCAN_CCCR_INIT_OFS;
// if (bo_bit == 1)
// {
// // 清除 INIT 位
// cccr_value &= ~MCAN_CCCR_INIT_MASK;
//
// // 将修改后的值写回 MCAN_CCCR 寄存器
// mcan_regs->MCANSS.MCAN.MCAN_CCCR = cccr_value;
// }
uint32_t ir_value = mcan_regs->MCANSS.MCAN.MCAN_IR;
uint8_t pea_bit = (ir_value & MCAN_IR_PEA_MASK) >> MCAN_IR_PEA_OFS;
if (pea_bit == 1 || bo_bit == 1){
//cccr_value &= ~MCAN_CCCR_INIT_MASK;
//mcan_regs->MCANSS.MCAN.MCAN_CCCR = cccr_value;
//DL_GPIO_setPins(GPIO_CAN1_STB_GRP_PORT, GPIO_CAN1_STB_GRP_PIN_CAN1_STB_PIN);
DL_MCAN_disablePower(MCAN0_INST);
delay_ms(1000);
DL_MCAN_enablePower(MCAN0_INST);
SYSCFG_DL_MCAN0_init();
hal_can_init();
//delay_ms(1000);
//cccr_value &= ~MCAN_CCCR_INIT_MASK;
//mcan_regs->MCANSS.MCAN.MCAN_CCCR = cccr_value;
//DL_GPIO_clearPins(GPIO_CAN1_STB_GRP_PORT, GPIO_CAN1_STB_GRP_PIN_CAN1_STB_PIN);
}
//uint32_t ir_value = mcan_regs->MCANSS.MCAN.MCAN_IR;
//printf("0x%x \r\n",psr_value);
//printf("0x%x \r\n",cccr_value);
//printf("0x%x \r\n",ir_value);
}
void hal_can_init(void)
{
xCAN_recv_Queue = xQueueCreate(CAN_QUEUE_LEN, CAN_QUEUE_SIZE);
if (NULL == xCAN_recv_Queue){
printf("CAN Queue err !\r\n");
}
/* Initialize global variables */
gServiceInt = 0; // Indicates whether the service interrupt is active
gInterruptLine1Status = 0; // Status of interrupt line 1
/* Clear GPIO pins for CAN1 standby */
// DL_GPIO_clearPins(GPIO_CAN1_STB_GRP_PORT, GPIO_CAN1_STB_GRP_PIN_CAN1_STB_PIN);
/* Enable MCAN0 interrupt in the NVIC (Nested Vectored Interrupt Controller) */
NVIC_EnableIRQ(MCAN0_INST_INT_IRQN);
/* Wait until MCAN0 enters normal operation mode */
while (DL_MCAN_OPERATION_MODE_NORMAL != DL_MCAN_getOpMode(MCAN0_INST));
}
这是我写的一个重新初始化MCAN模块的代码,在检测到pea或者bo被置位,会按照以下代码重置恢复,
DL_MCAN_disablePower(MCAN0_INST);
delay_ms(100);
DL_MCAN_enablePower(MCAN0_INST);
SYSCFG_DL_MCAN0_init();
hal_can_init();
但是,代码运行完之后CAN通讯并没有恢复,以下为寄存器的值,
MCAN_CCCR = 0x00000001
MCAN_PSR = 0x000007E7
MCAN_IR = 0x0A000000
总线依旧存在问题
添加cccr_value &= ~MCAN_CCCR_INIT_MASK;
mcan_regs->MCANSS.MCAN.MCAN_CCCR = cccr_value;去重置
CAN通讯并没有恢复,也会一直进入中断重新初始化MCAN模块
MCAN_CCCR = 0x00000000
MCAN_PSR = 0x0000070F
MCAN_IR = 0x00000000
CCCR.INIT重置后,寄存器虽然恢复正常,但是通讯依旧有问题,恢复不了CAN通讯
您觉得这代码哪里有问题,或者代码缺少了什么部分