This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LC4357: TMS570LC4357

Part Number: TMS570LC4357

请问大佬们,我用两块4357开发板进行CAN通信,我把他们分别都接到了stm32的收发器上了,并且以及将收发器++、--相连接,但是通过串口打印消息时一直显示收不到消息(两块板子都烧录了这个程序)

Fullscreen
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
void main(void)
{
/************************CAN Init**********************/
_enable_IRQ_interrupt_();
canInit();
canDisableloopback(canREG1);
canEnableErrorNotification(canREG1);
while(1)
{
can_mess(canREG1,canMESSAGE_BOX1,TEXT3);
}
}
void can_mess(canBASE_t *node, uint32 messageBox, uint8 * data_tx)
{
send_mess(node,messageBox,data_tx);
//canMessageNotification(node, canMESSAGE_BOX1);
printf("can ID is : %d",canGetID(node,messageBox));
printf("\r\n");
// receive_mess(node,messageBox,data_rx);
// sciDisplayText(sciREG1,&data_rx[0],sizeof(data_rx));
XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX