我是用的是STL76DN4LF7AG的NMOS,Rds=6 毫欧, VDS_LVL配置为0.2V, 应该保护的电流应该是33A,但是实际上在电机运行时6A左右就保护了,显示是VDS故障。
请问一下会是什么原因导致的

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我是用的是STL76DN4LF7AG的NMOS,Rds=6 毫欧, VDS_LVL配置为0.2V, 应该保护的电流应该是33A,但是实际上在电机运行时6A左右就保护了,显示是VDS故障。
请问一下会是什么原因导致的

1.GLx上的电容可能会减缓关断速度,但这可能并不是问题根源。弱上拉应该是MOSFET的体二极管正向导通导致的。
2.可能是MOSFET开通延迟差异导致并联管电流分配不均。