Part Number: DRV8243-Q1
We are currently using the SPI model of 8243. Sometimes the load current can reach the ITRIP regulation level, which will trigger some protection logic. I would like to ask if there is a recommended operating procedure when the load current reaches the threshold during the device operation. For example, should we first unlock the CONFIG register and then write to the CONFIG2 register to disable the current regulation?