This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8262: drv8262驱动电机互补的波形

Part Number: DRV8262


大家好 

设备使用DRV8262单H桥模式驱动电机,且配置如下:

原理图/配置:IN1与 MCU GPIO 相连、IN2与 GND 相连。 采用24V 电源时的开关频率为20kHz。

这意味着只能实现两个运行状态:正向和滑行(由于 IN2连接到 GND 并且始终为逻辑低电平)。

问题是:

IN1使用PWM驱动电机的时候,OUT1则是与IN1的波形相同,但是OUT2则出现了与OUT1互补的波形。不太明白为什么OUT2会出现互补的波形,OUT2的高是谁引起的,是电机电感产生的电压吗?