This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61288: TPS61288: How many parallel connections can be made at most? How to connect in parallel?

Part Number: TPS61288


Hello!

Does the boost support multiple parallel connections of progress, up to a maximum of several parallel connections?
I hope to output 12V when the input is around 3V, and I want to increase the output power of the system through parallel connection.