This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5148: 内部供电异常

Part Number: LM5148


设计指标:

输入电压:DC18V~DC50V

输出电压:15V

输出电流:3.3A

内部VDDA,VCC电压典型值为5V,电源输出电压为14.8V。电源运行一段时间后,空载输出电压只有4.5V,测量VDDA对PGND,VCC对PGND之间电压只有4.2V。技术规格书中并没有这个范围的值。请帮忙分析一下为什么VCC和VDDA只有4.2V,或者什么原因导致供电异常!我现在一脸茫然。

原理图见附件5383.DPS5024-015-NISO原理图.pdf