Part Number: LM25116
你好,使用TI在线工具设计的DC/DC转换器使用的主芯片LM25116,设计输入18~26V,输出的电压15V ,20A
目前测试情况接入1K电阻充当负载,输出电压3.67V,高边驱动信号2~7V之间-1.5~2V之间,VCC输出端电压7.2V,需要协助分析下是什么原因导致异常的,代入计算表格未发现明显异常
原理图:
高边及底边驱动波形

SW以及HB引脚电压波形

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.