This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25184: 请问输入端是否需要添加限流电阻呢

Part Number: LM25184

您好,我这边参照规格书使用LM25184进行了反激电源设计,输入为24V,输出功率合计约为7W,原边绕组电感为17uH。

与推荐设计的主要区别在于,为了限制上电时的冲击电流,我还在VIN之前还接入了1Ω的NTC电阻(尽管在规格书的推荐电路设计中,似乎并没有提到必需加入这种设计)。

至今,已制作了上百块电路板,其中有2块出现了首次上电即造成SW对GND短路的现象,更换LM25184芯片后即可正常工作。(其余大部分板子反复上电也不会有问题)

首先不排除是芯片个体的差异问题,但另一方面,我也在思考是否是设计问题。

我看规格书中提到,内部的MOSFET是2.5A的额定电流值。虽然电源回路中有原边电感,电流不会瞬时变化,但我无法定量去计算当前的设计数值是否会导致流过MOSFET的电流超标,才导致损坏了芯片。

麻烦帮忙分析一下原因,谢谢。

  • 您好,

    已经收到了您的案例,调查需要些时间,感谢您的耐心等待。

  • LM25184具有OCP(过电流保护),可防止初级峰值开关电流达到高于4.1A的值。如果出于任何原因触发此值,设备将降低其fsw=12kHz,输出电压将关闭,直到OCP条件消除,以防止MOSFET损坏和变压器饱和。话虽如此,您不需要NTC电阻器来限制初级侧的电流。详见数据手册说明。