Part Number: BQ40Z50
电池放电至3%的时候,插入充电器电量会跳到0再上升。这个会是什么原因引起的呀?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好
Is this right after programing golden image on the device? If so, right after programming the golden image, did they send the reset command, and do a quick discharge for the gauge to adjust to the new battery?
I took a closer look at their files, and see the FD bit gets set when the jump happens. If I remember correctly, there is a bit which does not allow the SoC to jump to 0% unless the FC threshold is reached. They cound modifty those, but I don't have the .gg file to confirm what is their settings. Can you share it?