BQ40Z50: BQ40Z50 R4电量跳变

Part Number: BQ40Z50


电池放电至3%的时候,插入充电器电量会跳到0再上升。这个会是什么原因引起的呀?

 

08efbf04b51b05e41ddfc6a1575f96fa.png

  • 您好,收到了您的案例,调查需要些时间,感您的耐心等待。

  • 您好

    这个问题可重复出现吗?如果可以,能否对BAT电压进行波形捕获?我想知道BAT电压是否出现振荡并导致FD位被置位。

    我们是否知道在此期间FD是否正在设置?

    您是否有这份数据日志可以分享?

  • 0777.BQ40Z50 R1 3% Drop.log附件为当时记录的跳变现象,后面满充一次之后再测试过六七次都没有再复现出来。

  • 您好

    Is this right after programing golden image on the device? If so, right after programming the golden image, did they send the reset command, and do a quick discharge for the gauge to adjust to the new battery?

    I took a closer look at their files, and see the FD bit gets set when the jump happens. If I remember correctly, there is a bit which does not allow the SoC to jump to 0% unless the FC threshold is reached. They cound modifty those, but I don't have the .gg file to confirm what is their settings. Can you share it?

  • 498174.TXT不知道为什么.gg.csv格式的文件上传不了。把.gg.csv改成.TXT就能。看看这样可以使用不?

  • 您好

    我能看到设置项。我发现他们的设置是仅在电量剩余0%时才触发FD(功能禁用)。他们本可以切换到基于电压的设置,但除非刚连接充电器时存在噪声,否则我不明白为何会出现这种情况。如果存在电压振荡,那么很可能是仪表突然检测到极低电压,从而强制将电量显示为零。

    如果他们在连接充电器前先松开电池,还能看到跳火吗?