Part Number: LM74810EVM
Other Parts Discussed in Thread: LM7481-Q1, LM74910H-Q1
您好,关于LM74810 在48V车载系统中,TVS的选型,请麻烦给出建议
- 运用在48V新能源车载系统,电池正常使用范围为40V到60V
- datasheet中推荐了12V系统和24V系统的TVS选型建议,请帮忙给出48V系统的TVS选型建议
- 请帮忙给出48V系统的MOSFET选型建议
感谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM74810EVM
Other Parts Discussed in Thread: LM7481-Q1, LM74910H-Q1
您好,关于LM74810 在48V车载系统中,TVS的选型,请麻烦给出建议
感谢
您好,
不好意思,这个帖子您没权限查看。
此贴是针对LM74910H-Q1器件的48V系统保护,讨论的结论是:
48V系统主要有一个70V的负载突波,不需要进行钳位,目前尚未发现已知的负电瞬变。
因此,从理论上讲,48V器件不需要TVS。
尽管如此,最好还是为TVS预留位置。
请添加两个SMBJ封装的单向TVS。