Part Number: SLUC222
Other Parts Discussed in Thread: UCC28950, TINA-TI
I am simulating a PSFB converter using UCC28950 in TINA-TI. My input voltage range is 43V to 58V and output voltage is 240-385V ,output power is 4KW. I am seeing an issue with the simulation output. The converter output voltage goes to 12V instead of 385V.
Issue: The output voltage doesnot change,It remains on 12V

Expected behavior: The converter should regulate at 365V as per the design tool for an input of 48 V.
What I have tried:
– Checked transformer turns ratio
– Adjusted compensation values
Simulational and design files are attached.
Could you please help for the detailed design and simulation using TINA TI simulation tool.
Thank you