This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5137: LM5137恒流模式下啸叫

Part Number: LM5137

我们的应用是启动电池的bms   用LM5137给电池充电   请求大佬们帮忙看看 
1、输入电压28V   恒流输出40A(两相单输出)  输出电压范围19-28     

2、为了实现恒流模式    我的设定的输出电压是29V   输入电压28V   电子负载CV模式26V 输出进行测试 

3、调试过程中遇到问题:用电子负载的CC模式可以正常输出       CV模式输出不正常,且啸叫很厉害

4、原理图SCH_Schematic2_2026-07-07.pdf 

5、PCB 嘉立创打开ProDoc_AUXBDCDC_TI_V1_2026-07-07.zip 

跪求大佬指点