This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25713BRSNT和BQ25713BRSNT相关问题



Dear All,

附件是原理图设计文件,烦请帮忙查看一下,目前电池使用2节锂电池,充满电压8.4V,电量5000mA/h。

另外有以下几个问题烦请帮忙确认一下。

电池电量计芯片:

1、电量计芯片配置参数,掉电需要重新初始化配置吗?

2、VEN/LEN管脚是否可以悬空?

3、电量计采样电阻电路是否正确?

电池充电芯片:

1、原理图中,Q2/Q3/Q5/Q6/Q7是否可以独立操作,通过I2C控制

2、电池充电时,VCC_BAT_SYS电源是否来自电池?

3、电池放电时,VCC_BAT_SYS是否从VCC_BAT+获取?

4、电池充放电是,VCC_BAT_SYS是否稳定输出?

5、电池放电保护之后,重新充电,需要重新初始化配置吗?

4237.file.pdf

Thanks!

  • 电量计芯片参数配置以后不会初始化参数,VEN/LEN不建议悬空,电流检测电路参考数据手册,您的电路上没有看到R-sense
    充电器芯片不独立控制Q2/Q3/Q5/Q6/Q7,充电时电源是外部adapter供电,放电是电池供电,输出电压稳定。放电保护之后,重新充电,不需要重新初始化配置
  • Dear Star,

    感谢您的回复;

    1、我理解,芯片内部有寄存器保存,掉电不丢失。是否这样?

    2、VEN与LEN,功能不用,管脚如何处理;

    3、R251是采样电阻,如下图:

    电池充电:

    下图中,Q5是一个PMOS管,充电时,电流流向电池。

    电池放电时,充电芯片是如何工作的,VCC_BAT+电流是如何流入充电芯片的?

    采样电流应该不是充电芯片的电流入口。别的管脚也没看到电池电流怎么流入充电芯片的。

    Thanks!