This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z80: BQ40Z80

Part Number: BQ40Z80

1.BQ40z80做容量学习时,充电充满了,但是FC一直没有置1,哪里配置不对吗?不知什么原因,有相关的人遇到此问题,方便解答一下!

SOC Flag config B默认的配置8c;

Charge term taper current设置500mA;

Chg Current Threshold=150mA;

Chg Current Threshold=10mA

通过阅读技术手册,上面写了在充电末端的时候FC置1的条件,以下条件均以达到但是仍然不见VCT置1和FC置1

  • 您好,请确认Mfg StatusInit[GAUGE_EN]是否使能,请参考TRM 5.7Chargeand DischargeTerminationFlags 配置TC 和FC的相关参数。

x 出现错误。请重试或与管理员联系。