This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51727: TPS51728+CSD87355两相电源冷启动上电出现台阶,热启动的时候台阶变小很多

Part Number: TPS51727


问题描述:

1,使用TPS51727+CSD87355的方案做成两相输出电源,输出电压为0.85V,最大电流支持50A,输入电压为12V,输出电压源主要给交换机MAC芯片CORE电源供电。目前测试发现冷启动上电过冲输出电压出现约100mV的台阶。帮忙分析下是什么原因?

在冷机启动的过程中,有发现输出电压0.85V在上电过程中出现大约100mV的台阶。如下图:

当TPS51727电源工作一段时间后,对TPS51727下电后又重新上电,台阶会减小很多,如下图。

cbb_tps51728_50a.pdf