This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV62130: 输出满载时,芯片的工作模式为什么还是PSM模式?

Part Number: TLV62130

1.如图为我们设计的原理图

2.我在进行输出满载测试输出电压纹波时,发现SW脚的波形是下图这种,看Datasheet上说这种是PSM模式,但是重载不应该是PWM模式吗?

(下面两张图中黄色为SW脚波形,蓝色为输出端纹波电压,第二张为时间轴拉短的波形)

3.这个是我按Datasheet上的公式算的在PSM模式下的输出负载电流(大约218mA)以及电感的峰值电流(435mA),请问计算有问题吗?