This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: 芯片进入shutdown状态,无法恢复

Part Number: BQ76952

您好: 

  我们在实现BQ76952的研发过程发现了一些问题:

 关于ALERT引脚,ALERT引脚作为ALERT功能时,产生一个报警信号,将ALERT PIN CONFIG配置为0x2A,同时ALERT引脚硬件上是上拉到3.3V,我们通过ALERT引脚产生的报警信号实现对MCU的控制,但是该信号确实有产生,但是运行一段时间之后芯片的AFE通信失效,无法采集电压电流数据,同时芯片进入到不是正常工作的状态,测量电流大小是7.1uA,且MCU无法控制采集芯片唤醒。请问下如果进入该种状态如何使芯片进入正常工作状态。从现象来看应该是软件程序上得问题,麻烦贵方提供一下技术指导。麻烦尽快给出答复,有些着急。

                                                                   peiqi wang

                                             2022.2.28

  • 您好我们已收到您的问题并升级到英文论坛,如有答复将尽快回复您。谢谢!

  • 麻烦发下国外E2E的解决方案链接即可,感谢!

  • 测试过后发现REG18存在1.8V电压,说明芯片处于是打开的状态,但功耗是只有18uA,且MCU始终无法与BQ通信,试过在LD两端给一个电压,依旧无法恢复到正常状态,请问RST_SHUTDOWN拉高一下或者是否可解决这种问题?还有是ALERT引脚在产生CUV报警之后只有从拉高的状态变为拉低的状态后一直保持拉低的状态,我们需要是在报警之后拉低之后还是报警清除后还是可以拉高,在测试过程中发现,清除报警后仍然保持低,且通过MCU手动恢复,仍无法使ALERT在拉低后再拉高,ALERT pinconfig寄存器配置为0x82同时关闭了protection的相关寄存器。如下图所示。

  • 已看到工程师的答复,现将原理图上传

    SHUTDOWN 如何恢复,在LD两端给到一个电压,仍然无法启动,将RST_SHUT引脚拉高一次,持续时间不超过1s发现BQ仍没有工作在正常状态。

    ALERT PIN 在ALERT功能是否可以配置为开漏模式

  • Luis H.S说:

    You mentioned that they measured 1.8-V in REG18, while power consumption remains low. It is possible that the device is stuck in "soft shutdown". Which can occur if TS2 is pulled low or if there's a voltage on the LD pin. Can they explain in detail what happens when they're having SHUTDOWN issues? If they reset the device does it get fixed? 

    BQ的TS2和LD电压在上电后都为0,同时通过MCU引脚在RST_SHUT引脚拉高,拉高后确实功耗变高了,但是BQ仍然无法通信。REG1确实有1.8V的电压。

    Luis H.S说:

    Are they using 100-Ohm for their sense resistors? This seems very high for a sense resistor. What discharge/charge currents do they expect? I also am concerned of the diodes used there, the diodes have a non-linear turn-on and can shift with temperature, so I am concerned that these would affect SRN/SRP measurements. The abs. max of the SRN/SRP pins are a minimum of -0.3-V to a maximum of 2.1-V. So you probably only need to worry about exceeding the absolute min.

    灵敏电阻是0.25毫欧,不是100欧,图中的R30和R178并联

    Luis H.S说:

    Ideally they should reference BAT- to Vss. Since they are not directly connecting to Vss, they should add a Schottky and Zener diodes on VC0 to keep it within the ABS maximum values

    请问下如果BAT-没有连接到Vss,需要增加肖特基二极管和齐纳二极管是为什么,请问这两个二极管的耐压值应该选择何种型号。. 

     Luis H.S未回答关于ALERT的问题。麻烦追问下这个引脚ALERT功能下是否可配置为开漏模式。

  • Luis H.S说
    Can they communicate if they use an EVM? If REG1.8 is on, the device should be awake. RST_SHUT should not be pulled high unless they want the part to go into SHUTDOWN or RESET.

    Luis 的意思是否是指使用评估板是否可通信是吗?我们使用的硬件是按照手册提供的电路图进行涉及,部分管脚有作修改,参照之前提供的原理图。REG18是存在的,REG1没有,保持RST高电平功耗有提升但是通信时关闭状态。在之前有提到过LD两端的电压和TS2两端的电压都为0,这是否会影响芯片进入到SOFT SHUTDOWN.

    Luis H.S说

    This can be configured in the Alert Pin Configurations. See Section 13.3.2.11 Settings:Configuration:ALERT Pin Config of the TRM.

    按照TRM中的配置在电池欠压的状态确实有产生一个脉冲信号,我们需要的功能是当外部有一个微弱的电流是,alert引脚是否也可产生一个interrupt信号给主机进程。如果想实现当外部有微弱电流时,ALERT可产生一个Interrupt信号给主机进程,请问如何实现

  • Luis H.S说

    Could they specify what you mean by weak external current? If using it as the ALERT configuration when there's a fault, there's no way to do this. Maybe if they set up this pin as a GPIO. They'll have to figure out the code to do this

    我们需要当电池进入充电状态下时,ALERT引脚产生一个脉冲,这个脉冲我们主要是用于可以唤醒MCU的,按照Luis H.S的建议,是否是将该引脚配置位GPIO的输出模式,然后当充电时,该引脚拉低再拉高

  • 您好,英文论坛已有相关答复,如您没有其他问题,我们会将该帖关闭。如您后续还需其他技术支持,欢迎您随时到论坛参与讨论,谢谢!