我依照Datasheet绘制了一块PCB 使用了TPS63060。
电感使用的是官方推荐的XFL1020-102ME
以下是电路图

PCB Layout是这样的

(请无视OUT方向写反的正负标识)
FB引脚的配置电阻中 R1为1MΩ 1% R2为110K 1%
二极管前的输出电压为5.54V
在带载之后,可调电源显示10V 0.1A,这时的输出电压掉到了5.2V
请问是什么原因导致了它的输出电压产生这样的下降?
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
电路比较简单,参考datasheet上的电路修改一下反馈电阻即可。
之后主要注意2个方面,功率电感饱和电流足够,其次layout上注意输入电容尽量靠近Vin脚,以及layout上功率回路尽量小,这些都容易造成带载后异常。(可以尽量参考datasheet)