This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63060: 带载掉压过大

Part Number: TPS63060

我依照Datasheet绘制了一块PCB 使用了TPS63060。

电感使用的是官方推荐的XFL1020-102ME

以下是电路图

PCB Layout是这样的 

(请无视OUT方向写反的正负标识)

FB引脚的配置电阻中 R1为1MΩ 1% R2为110K 1% 

二极管前的输出电压为5.54V

在带载之后,可调电源显示10V 0.1A,这时的输出电压掉到了5.2V

请问是什么原因导致了它的输出电压产生这样的下降?

谢谢