This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在电路设计中我需要解决以下问题:+12V电源输入的系统,通过DC/DC和LDO输出+3.3V和+5V,掉电时,需要+5V先掉电,电压至少掉至0.6V且最少持续50ms后,+3.3V后掉电。
1、在电压掉电到8V的时候,你关闭DC/DC及LDO,那么5V及3.3V输出就处于一个自然放电的过程,放电时间取决于输出电容的大小及负载等效阻抗。从简单的RC放电来看,越到后期,降低相同电压需要时间越长。
2、当电压掉到8V的时候,不要关闭LDO ,只关闭DC/DC。这样可以保证DC/DC自然掉电,而LDO还可以供电。
3、为了保证关闭DC/DC后,延长LDO的工作时间,可以适当增加12V输出的电容值。
首先感谢你的答复!
我现在需要在电压掉至+8V时迅速关断+5V,而保证+3.3V依靠剩下的能量维持50ms的工作时间。50ms间隔从+5V掉至0.6V开始,到+3.3V掉至+3V结束。
电容及外部模块的储能在掉电时能够维持至少100ms工作时间,因此迅速关断+5V至0.6V是关键。
我看TPS73601在EN管脚拉低后,在大部分情况下1ms内掉至0V,但实际测试并非如此,掉电极其缓慢需要接近40ms才掉至1.4V。
当电压降低到8V的时候,你即使关闭DC/DC,原来5V输出电压降低到0.4V的时间,取决于你5V电容与5V负载组成的RC放电时间常数,如果你的5V输出电容较大,负载较小,可能需要很长时间电压才能降低到0.6V。
你从TPS73601的PDF文档图24可以看到,如果输出电容及负载按照图上配置,应该在很短时间内电压降低到0V,问题是你目前的输出电容及负载分别是多少?
+5V正常工作时电流在200mA左右,等效电阻25欧,负载的旁路电容总共40uF,因此掉电时间应该不长。
但是IC不是纯阻性负载,电压降低后,电流降低速度更快。因此掉电变缓。
我增加或去掉100uF旁路后,对掉电似乎没影响,并且OFF掉EN管脚似乎也没影响。对比其他同方案电路板,掉电很迅速,我觉得是翻新芯片的可能性较大。
1、正常工作电流200mA,虽然是等效25欧姆,但可能电压降低到一定程度后,后面负载停止工作,因此电压降低将非常缓慢(你可以看以下5V电压波形,是不是到一定程度后电压下降不是按照RC指数图形开始下降,这个转折点应该是你后面负载停止工作的时刻。)
2、你看看你LDO,在OFF掉EN后,输出电压是不是同时刻开始下降,如果是跟翻新IC没有关系,我觉得你没必要关掉LDO,让他自然停止供电不完了吗?
1.无论我是否利用LDO的EN管脚,其输出电压下降的确是一直按指数形式下降的,但是掉压至1.4V后,RC时间常数变得很大,降压异常缓慢。EN管脚看似影响不大。
2.关断LDO后,LDO与DC/DC之间的电量大部分消耗在电源IC和分压电阻上,过程比较慢。不关断LDO,可能电压会掉的更快。但是EN管脚如果工作的话,我相信LDO电压会掉的更快。
我的意思是,如果在正常工作的时候,EN端能关闭LDO,那你目前的情况跟IC没有关系。电压掉到1.4V以后,RC时间常数变的很大原因在于你的负载在1.4V以后停止工作,放电属于输出滤波电容的自放电,所以时间常数很大。为什么说EN工作的话LDO电压会掉的更快?你指的这个电压是指LDO的输入还是输出?如果是输出,不关闭LDO,LDO输出应该持续时间更长才是。
讨论到现在我觉得可以确认的是:不管EN管脚是否给于关断信号,其带来的时间裕量都被1.4V以后时间给掩盖了,导致掉电时间达不到要求。问题的关键变成如何把1.4V停止工作的负载变成成0.6V才停止工作的负载。我接下来可能需要再做一些其他测试,再确定如何解决这个问题。十分感谢你热心的回复和专业精神!
对于LDO输出掉电会取决于输出电容,负载,和放电回路,所以为了加快电压下降,在不影响品质的条件下可以减小输出电容。对于LDO关断后,输出电压开始下降,前期取决于负载,但是到了一定时候,负载不在消耗能量则相当于断路,此时放电依赖放电回路,对于LDO的放电回路就是FB的分压电阻以及Vout内部的对地电阻80k, 外部分压电阻基于最好精准效果,使得其FB分压电阻(25kohm和79kohm)加起来是104kohm, 再与80kohm并联放电,等效的总放电电阻在45.2kohm, 对此有两个办法来加快放电,1是稍微牺牲一点精度降低FB的电阻,2就是额外再增加放电回路,例如在输出电容后加一个20~30kohm的电阻到GND, 这样的缺点在于多出1.25mW(以20k为例)的功耗。