This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5175: Iout=0电感啸叫和功耗大的问题

Part Number: LM5175


项目情况:Vin=9~32v ,Vout=18v ,Vsw=300KHz,Hicup off and DITH on,IOUT=0~3A.                                                                                           

现象:iout=0  电感在buck-boost工作状态下会啸叫.或者电感不啸叫输入电流会大于100mA,有时会出现电感和芯片温升高的问题.                                             

1.VCC 7.5V的电源要求是什么?现在测试芯片输出电压纹波大,约0.5·1v的三角纹波  .                    

2.Iout=0时,正常情况下在输入电压范围内最大的功耗是多少?目前测试有0.13A@10V,其余电压下最小也有50mA

3.输出电压纹波大,纹波0.6V@18V

4.我们调试过EVM板和wenben仿真参数,啸叫声只是大小的变化,功耗没有改变.