1,SOH,EOS模式中都有提到读取电池温度做参考,但是实际上芯片上的TS管脚无法去接电池本身的NTC管脚(电池的NTC电阻到GND,而参考原理图芯片上的TS管脚是将NTC上拉了),库仑计芯片毕竟在PCB板上,与电池内部的温度还是有差异的。比如设备刚开始大功率工作,PCB发热了,但是电池没有发热。此时库仑计获得的温度其实是PCB的温度,而不是电池的温度。这会不会导致EOS或者SOH得到的读数不准确?
2,如果我使用的是spec中的ACC模式,30分钟GE拉高一次(其余时间为低),测量电压,电流,温度等信息。我通过库仑计读到的信息,只是GE拉高时那个时间点的的电压,电流,和温度。并不能读取到30分钟内所有的时间连续不间断的放电活动和耗电信息。是吗?
3,如果我使用的是SOH模式(按照spec所说的8小时测量一次)是根据锂锰电池的电池电压,对照你们的database等到了当前电池的电量(SOH值),这个电量会很准确吗?精度高吗?8小时以内的所有连续不间断的放电活动我能监测到吗?
4,EOS模式是只针对亚硫酰氯电池使用,,根据电池内阻大小判断电池电量大小的模式。根据TI的文档,电池内阻只有在电池电量很低时才会有明显变化,其余时间没什么太大变化。这个模式可以精准的判断当前电池的电量吗?还是说只是判断电池接近没电了或彻底没电了?