This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76920: 1、BQ76920是否支持锂聚合物电池管理?2、运用BQ76920+BQ78350方案组装的锂聚合物电池板子与BQ24630充电板对接,很容易烧坏BQ24630;3、BQ76920+BQ78350方案组装的电池包在输出保护的情况下,与主板(含MCU)通过SMB接口对接,很容易烧坏MCU。

Part Number: BQ76920
Other Parts Discussed in Thread: BQ78350, BQ24630, BQ78350-R1A

电池组.pdf充电功能板.pdf 主板中集成的充电电路.docx我们用官方推荐电路搭建了BQ76920+BQ78350电池管理板(详见电池组.pdf)、充电功能板(详见充电功能板.pdf),还有在主板中集成了充电电路(与充电功能板中的电路一样,详见“主板中集成的充电电路.docx”)。问题1:最近我们用BQ76920+BQ78350电池管理板焊接组装了一个5节串联的锂聚合物电池包(每节最高电压4.35V),但用该锂聚合物电池包与主板中的充电电路对接时(详见“主板中集成的充电电路”,其中P2接口是与电池包接口),很容易将充电芯片BQ24630及周边元件烧坏,请问这是什么原因?问题2:我们还用BQ76920+BQ78350电池管理板焊接组装了一个5节串联的18650电池,当该电池包与主板对接时(详见“主板中集成的充电电路”,其中P2接口是与电池包接口),在输出保护的情况下,很容易将MCU烧坏,此时,我们监控了SMB线路上BQ76920+BQ78350电池管理板一端电阻上的温度,发现温度一直往上飙升,说明SMB线路上的电流很大,请问这是什么原因造成的?

  • 您好,附件的主板集成充电电路文件无法打开。其他问题正在查看

  •  这是主板中集成的充电电路,文件被加密了,打不开。

  • 您好,由于问题比较复杂,我需要询问更了解这款芯片的TI工程师,再帮您解答,稍后回复。

  • 您好,This schematic does not show very much - it only shows the pull-up resistors for the SMB_CLK and SMB_DAT. Maybe it is possible something is shorted near the P2 connector - the power connections (BAT+ and PACK-) are sharing the same connector with the SMBUS pins.

  • 您好,BQ24630有两个电路,看起来不是一个电路。

    您能否说明IC损坏时的测试条件以及其他哪些组件损坏?

  •  这是主板中的MCU部分电路,MCU与电池包通过SMB_CLK、SMB_DAT连接。烧坏MCU时的测试条件:我组装的一个5节18650串联的电池包与主板连接(通过P2接口,即BATT+、PACK-、SMB_CLK、SMB_DAT等4个引脚对应连接),此时,将AOLD、 ASCD的“Threshold and Delay”值均设为0,电池输出保护(应是短路保护),保持电池包与主板连接几分钟,MCU便会烧坏。后来,我们加大了串在SMB线路上的电阻(下图中的R36、R38)阻值(均改为510R),在相同的条件下复现上述问题,监测电阻温度会一直上升。

  • 另一个烧坏充电管理芯片问题测试条件: ,我用BQ76920+BQ78350电池管理板焊接组装了一个5节串联的锂聚合物电池包,如上图所示。用该电池包管理板与主板对接(通过P2接口,即BATT+、PACK-、SMB_CLK、SMB_DAT等4个引脚对应连接),电池管理板接上主板瞬间便会将主板中集成的充电电路中的BQ24630芯片及其周边元件烧坏,如下图中箭头所指。该锂聚合物电池管理板与主板反 复多连接/断开几次,烧坏现象很容易复现。(注:正常情况下,电池包一直有电压输出,锂聚合物电池管理板与主板连接属带电插拔)

  • BQ24630有两个电路:用“主板中集成的充电电路”分析问题,上传的“充电功能板.pdf”只是为了参考(把这部分充电管理电路整体移入主板中,只是位号不同而已)。

  • 您好,I do not see anything in the schematic that explains why the microcontroller is getting damaged. I do not think this is caused by the SMBus lines since these lines are driven by the STM32 (host) and not the BQ78350-R1A. They need to figure out where the damage is occurring on their microcontroller and why. I do not think this is related to the TI devices.

  • 您好,This issue is most likely caused by voltage ringing above the absolute max of the device from the hot plug.

    My suggestions will be 1) using the adapter hot plug snubber circuit (see below, but you will need a large resistor as there will be current going through multiple times due to constant hot plug), or 2) use a TVS diode to clamp the ringing (recommended).

  • 您好!烧坏MCU的问题肯定与电池管理芯片接口设计有关,关键问题见图中红字描述。

  • 您好,建议您检保护时SMB线路上的电流是哪里来的,从而确认是哪里的问题。