This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Output 60V/1.5A then close the input of LM5121 for 0.5s,after restart the LM5121 is working abnormal,the output is what the input is,and the Switch is not work;Could see the voltage of Vss is grow up slowly under 1.2V during 4.5s
Hi
可以先用在线仿真webench确认一下电路。
其次layout上注意一下sense电阻,避免noise导致导致电流保护。 以及功率电感饱和电流适当放大一些,输入电容足够大靠近电感、
Hi Johnsin
我能够稳定复现该问题,通过在lm5121输出级提前上电(60V),然后再给LM5121输入级上电,就会出现这种Vss波形的异常;请问这个状态是芯片内部那个部分导致的呢? 是否异常呢
请问这部分可以详细讲一下吗?我这边默认最低输出是28V,但是当我在输出提前上49V都是可以正常启动的,当拿掉输出的49V,可以看到输出会稳定在28V;然后这个负载是电池,就出现这个问题了