This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Output 60V/1.5A then close the input of LM5121 for 0.5s,after restart the LM5121 is working abnormal,the output is what the input is,and the Switch is not work;Could see the voltage of Vss is grow up slowly under 1.2V during 4.5s
Hi
可以先用在线仿真webench确认一下电路。
其次layout上注意一下sense电阻,避免noise导致导致电流保护。 以及功率电感饱和电流适当放大一些,输入电容足够大靠近电感、
Hi
升压获得的输出小于已有的输出导致芯片启动异常,这种情况一般不会出现在实际带载情况,你可以将反馈电阻等比率较小加快输出放电看看?