This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Output 60V/1.5A then close the input of LM5121 for 0.5s,after restart the LM5121 is working abnormal,the output is what the input is,and the Switch is not work;Could see the voltage of Vss is grow up slowly under 1.2V during 4.5s
Hi
可以先用在线仿真webench确认一下电路。
其次layout上注意一下sense电阻,避免noise导致导致电流保护。 以及功率电感饱和电流适当放大一些,输入电容足够大靠近电感、
Hi Johnsin
你初步怀疑是保护那边的么? 我这边有测试Vres的波形,没有变化,为了兼容5122所以把过流给屏蔽了,触发circuit breaker不会进行Switch;目前抓了Vres,没有抬高,反而是启动时序的Vss没有按照正常的波形进行,我晚一点把波形上传一下;(虽然看起来就像触发了circuit breaker的表现,但是这发生在启动时);目前电源部分测测试过,都比较稳定,偶然发现有这个问题
Hi Johnsin
我能够稳定复现该问题,通过在lm5121输出级提前上电(60V),然后再给LM5121输入级上电,就会出现这种Vss波形的异常;请问这个状态是芯片内部那个部分导致的呢? 是否异常呢