This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25606: 0-10或者45-60度sta指示问题

Part Number: BQ25606


1、问题背景:12月初开始,插件握把陆续有供货商反馈电池充电10h~12h红灯依旧不熄灭。

2、问题分析: (1)此产品之前已陆陆续续出货,从仓库抽检40台,室温环境下均无充满电后红灯不熄灭的情况,10度以下复现了红灯不会熄灭的情况。

查找手册,发现以下一处可以解释此现象:

手头2019年的规格书如下

在TI官网下载最新的规格书如下

可以看到最新的规格书加了这一句:Charge termination is disabled for cool and warm conditions

也就是在0~10度和45~60度时充电终止这个功能是不起作用的,也就是STAT不会变高,这也解释了红灯为什么不会熄灭。

  • 本次测试共测试两个型号,测温产品线的手机插件握把、户外的AFFO
  • 现象具体如下:如果是10度以上电池充满了灯灭了,此时再降到0~10度红灯不会再亮起,
  • 但是如果此时再拔掉USB再插上,红灯就会一直亮。45度以上则表现为红灯一直闪烁。
  • 是否可以确认这是芯片本身就是这样设计的,同时低温0-10时候或者高温45-60度,各使用BQ25606的项目都会有此问题,sta指示灯不正确问题。