This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

采用tps55340升压,tps54331降压,负载1.5A没问题,负载2.0A不行?

Other Parts Discussed in Thread: TPS55340, TPS54331, TPS54340

TI工程师:你好,我采用tps55340升压,tps54331降压,输入的电源是15V,4A,期望输出的电压是12V,能够带动3A的负载,电路设计是参照数据手册设计的。

在测试过程中,当负载的电流是1.5A时,电压是可以带动负载的,但是当负载的电流增大时(大于1.5A,1.6A),电压就自动断电了。

 电感:CDRH103RNP-2R2N   6.7A, 16.9 mΩ

电感:CDRH103RNP-6R8N  3.84A, 35 mΩ

B540C  肖特基二极管,5 A, 40 V