This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS755: 大电流应用

Part Number: TPS755
Other Parts Discussed in Thread: TPS7A53,

最近一个项目想使用TPS75533KTT,但是由于是大电流应用不知道是否可用,想请教一下。

输入电压为5V时,输出为3.3V,此时压降为1.7V,按手册上最大电流5A计算,芯片上的发热功率为8.5W,

换算成温升即328℃(手册上的参数为底部不铺铜散热),已经远远超过芯片的工作温度。

这种情况我应该如何使用才能让芯片的电流达到5A呢?板子做好散热就行了吗?