你好,现有设计中使用5.5V输入。输出±5V电压,反馈电阻分别为(150K/475K和150K/470K),Ccp为4.7uF,C1为1uF,Cvin为4.7uF和2.2uF并联,Cout暂时都使用了3个1uF并联
- 测试发现正压负压的TR(10%~90%)不同,正压40us左右,负压3ms左右,数据表没有给出此项数据。
- 负压输出端纹波较大(30mV以上),打算串联磁珠,利用LC滤波,可以给一下选型的建议吗。
- PGOOD功能在不使用的情况下,悬空还是接地。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,现有设计中使用5.5V输入。输出±5V电压,反馈电阻分别为(150K/475K和150K/470K),Ccp为4.7uF,C1为1uF,Cvin为4.7uF和2.2uF并联,Cout暂时都使用了3个1uF并联
Hi
1. 这款芯片并没有像其它芯片那样有明确的软起动控制来表明启动时间,规格表中也没有明确的规格,不过datasheet第7页的图10有启动波形,从波形判定启动时间低于50uS(如果每格是200uS).
2,磁珠加4.7uF电容即可。
3. Powergood不用悬空即可。