This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM27762: 1.datasheet没有看到正负压的Start-up time。2.LM27762的负压输出端使用磁珠来滤波如何选型?3.PGOOD功能的问题。

Part Number: LM27762

          你好,现有设计中使用5.5V输入。输出±5V电压,反馈电阻分别为(150K/475K和150K/470K),Ccp为4.7uF,C1为1uF,Cvin为4.7uF和2.2uF并联,Cout暂时都使用了3个1uF并联

  • 测试发现正压负压的TR(10%~90%)不同,正压40us左右,负压3ms左右,数据表没有给出此项数据。
  • 负压输出端纹波较大(30mV以上),打算串联磁珠,利用LC滤波,可以给一下选型的建议吗。
  • PGOOD功能在不使用的情况下,悬空还是接地。