This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2576HVS-ADJ 为何 带风机负载 电压降低



HI 您好

LM2576HVS-ADJ 应用中遇到问题 输入电容100uF /63V  电感100uH/3A; 输出电容2200uF 63v 肖特基SS34  ;输入 电源:48V 5A;

 负载为 调压调速  风机  调节反馈段R2=33.2K R1=1K 无负载时 输出电压是1.23*(1+R2/R1);

为何风机运行时     输出电压下降到40.3V 左右?

风机最大电流  0.6A  48V

 

  电路见附件

 

Thanks and best regards