This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5122: 输出电压与输入电压几乎相等,无法满足输出电压为60V的设计。

Part Number: LM5122

N0.1:如图1所示,采用WENBENCH建议的设计,结果是输出电压与输入电压相差不到1V,无法升压。怎么解决呢?备注:设计目标是输入电压为:15V-60V,输出电压为60V,最大输出电流为1A。

NO.2:我是用万用表测量输出电压的,这样测量是否能够测到输出电压为60V?如果不能测到,那该用什么测量?

NO.3:在将LM5122引脚实际电压与Pspice直流偏置仿真对比,发现SLOPE有区别,实际:SLOPE=0V,仿真:SLOPE=1.2V。这个差异说明什么问题呢?

最后,我该怎么做才能升压?