This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ28Z610-R1: BQ28Z610-R1

Part Number: BQ28Z610-R1
Other Parts Discussed in Thread: GPCCHEM, BQSTUDIO, BQ28Z610

BQ28Z610-R1电量无法更新,一直是100%。我这边把GG文件上传给你这边,请帮忙看一下什么原因。ID为7349.谢谢!

DRT-31K1008.gg.csv

  • 您好,请将register画面发过来看一下RM  和FCC的值。

  • 目前在充电中,但是一直显示100%

  • 您好,画面上看FCC一直是0,所以RSOC不更新,您的CHEM ID是否通过GPCCHEM tool 帮助您计算。

  • Chemistry ID selection tool, rev=2.54		
    		
    Configuration used in present fit:		
    ProcessingType=2		
    NumCellSeries=1		
    ElapsedTimeColumn=1		
    VoltageColumn=2		
    CurrentColumn=3		
    TemperatureColumn=4		
    		
    Best chemical ID : 7349	Best chemical ID max. deviation, % : 0.98	
    		
    		
    		
    Summary of all IDs with max. DOD deviation below 3%		
    		
    Chem ID	max DOD error, %	Max R deviation, ratio
    7349	0.98	0.31
    2939	1.12	0.51
    576	1.27	0.48
    5753	1.27	0.5
    7456	1.27	0.33
    5154	1.31	0.6
    1807	1.46	0.72
    2445	1.68	0.71
    2146	1.78	2.44
    7121	1.87	0.16
    5459	1.97	0.62
    5906	2.01	1
    7102	2.05	0.74
    5747	2.09	0.75
    5257	2.12	0.7
    2897	2.2	0.8
    2782	2.21	0.66
    7227	2.21	0.82
    7112	2.25	0.7
    7183	2.26	0.98
    7176	2.4	0.6
    7422	2.42	0.57
    5665	2.44	0.86
    7394	2.45	0.75
    5945	2.66	0.96
    2038	2.84	1.24
    5604	2.86	0.72
    5792	2.89	0
    2987	2.91	1
    2064	2.93	0.59
    2408	2.96	1.15
    		
    Max. deviations for best ID is within recommended range. Chosen best chemical ID is suitable for programming the gauge.		
    		
    		
    Selection of best generic ID for ROM based devices like bq274xx		
    		
    		
    Device / Family #1		
    Generic Chem ID	Device/ Voltage/ Chemistry	max DOD error, %
    3142	bq27421-G1D: 4.4V LiCoO2	16.38
    354	bq27411-G1C: 4.35V LiCoO2	18.9
    128	bq27421-G1A: 4.2V LiCoO2	24.28
    312	bq27421-G1B: 4.3V LiCoO2	28.48
    Best generic ID 3142		
    Warning: Generic ID Deviation is so high that it is most likely due to anomaly in the data. Please check that data files have recomended format, units and test schedule		
    		
    		
    Device / Family #2		
    Generic Chem ID	Device/ Voltage/ Chemistry	max DOD error, %
    1210	bq27621:  (ALT_CHEM1) 4.3V LiCoO2	17.62
    354	bq27621:  (ALT_CHEM2) 4.35V LiCoO2	18.9
    1202	bq27621: (default) 4.2V LiCoO2	19.26
    Best generic ID 1210		
    Warning: Generic ID Deviation is so high that it is most likely due to anomaly in the data. Please check that data files have recomended format, units and test schedule		
    		
    		
    Device / Family #3		
    Generic Chem ID	Device/ Voltage/ Chemistry	max DOD error, %
    3142	bq27426: (ALT-CHEM2) 4.4V LiCoO2	16.38
    3230	bq27426: (default) 4.35V LiCoO2	18.9
    1202	bq27426: (ALT_CHEM1) 4.2V LiCoO2	19.26
    Best generic ID 3142		
    Warning: Generic ID Deviation is so high that it is most likely due to anomaly in the data. Please check that data files have recomended format, units and test schedule		
    		
    		
    Warning: voltage in V detected	 divider changed to 1	
    

    我试过3个ID,都是一样

  • 帮忙看一下,这个是电路图,单节电池的,两节电池之前没有出现这些问题

  • 感觉不是ID问题,因为我不变ID,复位一次就是100%,只要复位就会变成100%

    毕竟这个肯定还需要更加电压来判定相对容量的。而且总是发现PACK pin voltage比BAT pin voltage及Cell 1 voltage 要高很多。这样很容易进入保护状态。

  • 您好,请确认QMAX是否更新,如果电池未充电或放电,这些值往往会报0。 是否已经制作golden 文件? 如果没有,可以在下面找到完成此操作的过程:

    https://www.ti.com/lit/pdf/slua777 

  • 但是我这个版本好像不需要制作golden文件。上面没有制作golden文件的按钮,其他的版本是有的。很奇怪。

  • 我先按要求去做循环

  • 您好,固件版本不同BQstudio会有些按键区别。可以通过firmware 按钮导出golden文件。

  • 参考使用手册,在设置[FAST_QMax_LRN] = 1的时候, 会变为06.但是还是04.

    这个太奇怪了。

  • 您好,update status是学习成功才会更新。当更新状态 = 06 时,Fast_QMax_LRN使能表示在学习周期期间启用快速 QMax 。

  • 现在有一个问题是,只要去掉IIC通讯,等2分钟后就不能充电,插上通信就立马能充电。这个有开关设置吗

  • Bq28z610能通过固件升级到BQ28Z610-R1吗

  • 您好

    只要去掉IIC通讯,等2分钟后就不能充电

    请确认SLEEPCHG的设置

    Bq28z610能通过固件升级到BQ28Z610-R1吗

    可以通过固件升级到BQ28Z610-R1

  • 现在状态能更新了,但是碰到一个怪异的问题,就是registers中的charging  voltage 和charging current显示的竟然是rec temp charging.这个非常怪异,和之前的一下IC完全不一样。见附件,这个大概是什么原因造成的。

    谢谢

    问题点.pdf

  • Cell 1 Chg Voltage at EoC

    Cell 2 Chg Voltage at EoC

    你看一下这两个位置的参考不对,填上电芯的充电上限电压。

  • 您好,这两个参数是充满电的充电电压。

    rec temp charging请参考TRM 4.4 Charging Current

  • 现在还有一个问题没有解决,就是无负载的时候,输出电压比如是4.1V,但是无负载时,电压会掉落到3.3V左右,一带载超过阈值电流就可以恢复,应该是充电mos关闭了,这个在哪里可以设置。

  • 您好,

    无负载的时候,输出电压比如是4.1V,但是无负载时,电压会掉落到3.3V左右,一带载超过阈值电流就可以恢复,应该是充电mos关闭了

    电压掉落看一下register画面有什么异常。