Other Parts Discussed in Thread: GPCCHEM, BQSTUDIO, BQ28Z610
BQ28Z610-R1电量无法更新,一直是100%。我这边把GG文件上传给你这边,请帮忙看一下什么原因。ID为7349.谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
BQ28Z610-R1电量无法更新,一直是100%。我这边把GG文件上传给你这边,请帮忙看一下什么原因。ID为7349.谢谢!
Chemistry ID selection tool, rev=2.54 Configuration used in present fit: ProcessingType=2 NumCellSeries=1 ElapsedTimeColumn=1 VoltageColumn=2 CurrentColumn=3 TemperatureColumn=4 Best chemical ID : 7349 Best chemical ID max. deviation, % : 0.98 Summary of all IDs with max. DOD deviation below 3% Chem ID max DOD error, % Max R deviation, ratio 7349 0.98 0.31 2939 1.12 0.51 576 1.27 0.48 5753 1.27 0.5 7456 1.27 0.33 5154 1.31 0.6 1807 1.46 0.72 2445 1.68 0.71 2146 1.78 2.44 7121 1.87 0.16 5459 1.97 0.62 5906 2.01 1 7102 2.05 0.74 5747 2.09 0.75 5257 2.12 0.7 2897 2.2 0.8 2782 2.21 0.66 7227 2.21 0.82 7112 2.25 0.7 7183 2.26 0.98 7176 2.4 0.6 7422 2.42 0.57 5665 2.44 0.86 7394 2.45 0.75 5945 2.66 0.96 2038 2.84 1.24 5604 2.86 0.72 5792 2.89 0 2987 2.91 1 2064 2.93 0.59 2408 2.96 1.15 Max. deviations for best ID is within recommended range. Chosen best chemical ID is suitable for programming the gauge. Selection of best generic ID for ROM based devices like bq274xx Device / Family #1 Generic Chem ID Device/ Voltage/ Chemistry max DOD error, % 3142 bq27421-G1D: 4.4V LiCoO2 16.38 354 bq27411-G1C: 4.35V LiCoO2 18.9 128 bq27421-G1A: 4.2V LiCoO2 24.28 312 bq27421-G1B: 4.3V LiCoO2 28.48 Best generic ID 3142 Warning: Generic ID Deviation is so high that it is most likely due to anomaly in the data. Please check that data files have recomended format, units and test schedule Device / Family #2 Generic Chem ID Device/ Voltage/ Chemistry max DOD error, % 1210 bq27621: (ALT_CHEM1) 4.3V LiCoO2 17.62 354 bq27621: (ALT_CHEM2) 4.35V LiCoO2 18.9 1202 bq27621: (default) 4.2V LiCoO2 19.26 Best generic ID 1210 Warning: Generic ID Deviation is so high that it is most likely due to anomaly in the data. Please check that data files have recomended format, units and test schedule Device / Family #3 Generic Chem ID Device/ Voltage/ Chemistry max DOD error, % 3142 bq27426: (ALT-CHEM2) 4.4V LiCoO2 16.38 3230 bq27426: (default) 4.35V LiCoO2 18.9 1202 bq27426: (ALT_CHEM1) 4.2V LiCoO2 19.26 Best generic ID 3142 Warning: Generic ID Deviation is so high that it is most likely due to anomaly in the data. Please check that data files have recomended format, units and test schedule Warning: voltage in V detected divider changed to 1
我试过3个ID,都是一样
帮忙看一下,这个是电路图,单节电池的,两节电池之前没有出现这些问题
感觉不是ID问题,因为我不变ID,复位一次就是100%,只要复位就会变成100%
毕竟这个肯定还需要更加电压来判定相对容量的。而且总是发现PACK pin voltage比BAT pin voltage及Cell 1 voltage 要高很多。这样很容易进入保护状态。
您好,请确认QMAX是否更新,如果电池未充电或放电,这些值往往会报0。 是否已经制作golden 文件? 如果没有,可以在下面找到完成此操作的过程:
您好,update status是学习成功才会更新。当更新状态 = 06 时,Fast_QMax_LRN使能表示在学习周期期间启用快速 QMax 。
您好
只要去掉IIC通讯,等2分钟后就不能充电
请确认SLEEPCHG的设置
Bq28z610能通过固件升级到BQ28Z610-R1吗
可以通过固件升级到BQ28Z610-R1
您好,
无负载的时候,输出电压比如是4.1V,但是无负载时,电压会掉落到3.3V左右,一带载超过阈值电流就可以恢复,应该是充电mos关闭了
电压掉落看一下register画面有什么异常。