This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
When I tesing my design board for TPS552892.
The efficiency does not meet specifications definition.
Test data1 _(PFM_5Vin/ 5vout):
Test data2 -(FPWM_(5Vin/ 5vout)):
But, When I change the VIn to 20V(Keep Vout : 5V)
The measurement data is close to the specification information.
Test data2 -(FPWM_(20Vin/ 5vout)):
As far as I know, 558892 duty cycle can be 100%,
Why is it so bad of Efficiency for 5vin/5vout?
Hi
输入输出接近时效率偏低较多,建议你严格参考datasheet, 因为此时芯片转换模式可能存在不稳定导致效率偏低。
第三个设计是降压,效率也有些偏低,建议你选择选择更低DCR的功率电感。
另外你工作频率选择多少,一般不建议太高,300kH~400kHz即可。